ProtectNet PTEL2 OR PNET1GB ??

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • ProtectNet PTEL2 OR PNET1GB ??
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
Administrator BillP Administrator
2151
Teken
Kirk Teken
123
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
Back to APC UPS for Home and Office Forum
Start a Topic
Anonymous user
Not applicable

Posted: ‎2021-06-28 08:04 AM . Last Modified: ‎2024-03-26 03:42 AM

0 Likes
0
795
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
Posted: ‎2021-06-28 08:04 AM . Last Modified: ‎2024-03-26 03:42 AM

ProtectNet PTEL2 OR PNET1GB ??

I have a phone/internet connection FTTC VDLS2 (bandwidth frequency: 17-35 MHz), with a "Technicolor 768600" gateway (router+modem).
On the wall there's an outlet with 2 phone jacks (RJ-11 ports); a light gray cable comes out of the 1st port, with only 2 wires and the two central pins (n. 2 and 3), which plugs into the gateway VDSL2 port ; from the other port of the outlet a black cable comes out, always with only 2 wires and two central pins (n. 2 and 3), which plugs into the gateway LINE 1 port (IN).
At the gateway LINE 2 port (OUT) a phone cable connects a fax modem inserted into my PC, a fax machine / printer multifunction to which the telephone and the t.a.m. are connected.
The gateway PSTN port is empty.
The gateway Ethernet port 1 is connected, by an Ethernet cable, to my Switch port 1. To the other 7 Switch ports the various network devices are connected: PC, scanner, etc.

To protect the fax modems, the gateway (router+modem) and the ethernet/switch network from overvoltages, do I have to use the APC ProtectNet for phone lines PTEL2 OR the ProtectNet for Ethernet lines PNET1GB ? Or both of them?
Where should I mount it/them ?
Thanks for the tips.

Labels
  • Labels:
  • Back-UPS & Surge Protectors
  • Tags:
  • gateway
  • modem
  • overvoltage
  • protectnet
  • router
  • surge
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.