Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84244members
353343posts

ProtectNet PTEL2 OR PNET1GB ??

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Mrmind_apc
Crewman
Crewman
0 Likes
0
153

ProtectNet PTEL2 OR PNET1GB ??

This was originally posted on APC forums on 7/11/2019


I have a phone/internet connection FTTC VDLS2 (bandwidth frequency: 17-35 MHz), with a "Technicolor 768600" gateway (router+modem).
On the wall there's an outlet with 2 phone jacks (RJ-11 ports); a light gray cable comes out of the 1st port, with only 2 wires and the two central pins (n. 2 and 3), which plugs into the gateway VDSL2 port ; from the other port of the outlet a black cable comes out, always with only 2 wires and two central pins (n. 2 and 3), which plugs into the gateway LINE 1 port (IN).
At the gateway LINE 2 port (OUT) a phone cable connects a fax modem inserted into my PC, a fax machine / printer multifunction to which the telephone and the t.a.m. are connected.
The gateway PSTN port is empty.
The gateway Ethernet port 1 is connected, by an Ethernet cable, to my Switch port 1. To the other 7 Switch ports the various network devices are connected: PC, scanner, etc.

To protect the fax modems, the gateway (router+modem) and the ethernet/switch network from overvoltages, do I have to use the APC ProtectNet for phone lines PTEL2 OR the ProtectNet for Ethernet lines PNET1GB ? Or both of them?
Where should I mount it/them ?
Thanks for the tips.