Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84777members
354220posts

Powerchute with Back-UPS 1500 (BN1500M2-CA) Auto shutdown after PC hibernate

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

mduvy
Cadet
0 Likes
0
213

Powerchute with Back-UPS 1500 (BN1500M2-CA) Auto shutdown after PC hibernate

I have a PC (with data cable going to UPS), a Raspberry Pi and IP switch connect to my UPS. I configured in PowerChute Personal Edition v3.1.0 to hibernate the PC after 2 minutes running on the battery. I want to keep the battery autonomy for the Raspberry Pi and IP switch. When the UPS go on the battery, I see ~120 minutes of autonomy remaining on the UPS for the PC, Raspberry Pi and IP switch. After 2 minutes the PC will hibernate, once the PC is off the autonomy go up to ~300 minutes. ~2 min after the PC is powered off, the UPS will shutdown by itself.

 

Any idea how to solve this? I think the issue is in PowerChute. We should have the option to not turn off the UPS once the PC is powered off.

 

I made few tests when the UPS go on the battery:

  • After the PC is powered off and the UPS auto shutdown, if I power on back the UPS on battery olny, the UPS will run with the Raspberry Pi and IP switch until battery died.
  • If I change the parameter in PowerChute to hibernate the PC when there is 5 minutes left on the battery. The PC will hibernate as expected, the UPS battery will increase but the UPS will auto shutdown ~2 minutes after the PC is powered off.
  • If I remove the data cable between PC and UPS before putting the UPS on battery. The PC will not hibernate, and all equipment will stay up until battery is dead.