Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84473members
353690posts

Powerchute Personal Edition 3.0 - apcsystray.exe permissions startup bug

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
barnabyr_apc
Ensign
Ensign
0 Likes
3
295

Powerchute Personal Edition 3.0 - apcsystray.exe permissions startup bug

This was originally posted on APC forums on 10/28/2010


I just upgraded to Powerchute Personal Edition 3.0 from 2.2 today on 2 Win7 x64 boxes. Have Back-UPS XS (RS) 1000, Firmware revision: 7.g8.D. Now, every time I log in, I get a Windows UAC window pop up asking for admin permissions to allow apcsystray.exe (system tray icon) to make changes to the system. Even if I login as admin, a UAC window pops up. Standard users must click no to get rid of the window. If admin pword is entered, the system tray icon appears, and can be used to change powerchute settings. If not, no system tray icon. Even if "Always show icon in system tray" option is unchecked, the annoying UAC window still pops up, although, if one enters admin pword, no tray icon will appear.

These windows are a useless hassle. How can I turn them off and return to 2.2 behavior, which was that the UAC window will appear only if the systray icon is double-clicked?

Thank you...
___________________________
Alienware Area 51 X58
ASUS X58 P6T Deluxe motherboard with integrated sound (SoundMAX)
Core i7 940 2.93 GHz
6 GB DDR3 RAM 1333MHZ (3 x ELPIDA 2GB DDR3 1333MHZ JEDEC STANDARD PC3-1066)
NVIDIA GTX 295 (2 PCB), no overclock, Video BIOS: 62.00.4E.00.02
Win 7 x64
Dell 2408WFP monitor, 1920x1200, 59 (60) Hz
WESTERN DIGITAL 300GB 10K SATA HDD REV2 main hard drive
1000 watt power supply

Message was edited by: barnabyr


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
296

Re: Powerchute Personal Edition 3.0 - apcsystray.exe permissions startup bug

This reply was originally posted by Angela on APC forums on 9/7/2011


h1. this is now fixed!

PCPE version 3.0.0.1 is now available on the web. This is an interim release that is available in English & German and addresses three major concerns.

Fixes in this release:*

•With Windows UAC enabled, when a user logged on to Windows Vista or Windows 7, the UAC dialog always asked the user to approve starting the PowerChute Systray icon. This will no longer happen.

•After un-installing PowerChute, hibernation was not being restored and has been corrected.

• When selecting PowerChute Technical data screen it would be displayed very slowly and sometimes the internal PC fan made a lot of noise (indicating over usage). This has also been addressed.

Here is the link to the software or you can browse to it on apc.com/tools/download

http://www.apc.com/tools/download/software_comp.cfm?sw_sku=SFPCPE3001

See Answer In Context

3 Replies 3
barnabyr_apc
Ensign
Ensign
0 Likes
0
297

Re: Powerchute Personal Edition 3.0 - apcsystray.exe permissions startup bug

This was originally posted on APC forums on 10/29/2010


Apparently, apcsystray is set by default to "run as administrator". I cannot change that behavior by editing permissions/ownership. Proper behavior should be that the .exe should NOT startup as admin, requiring password, but that, when the tray icon is clicked, it would THEN ask for admin permissions to run the main APC GUI to change system settings.

What was the rationale for changing this behavior in 3.0?

Message was edited by: barnabyr

BillP
Administrator Administrator
Administrator
0 Likes
0
297

Re: Powerchute Personal Edition 3.0 - apcsystray.exe permissions startup bug

This reply was originally posted by Angela on APC forums on 10/29/2010


hi

we already have a thread, [started here|http://forums.apc.com/spaces/4/back-ups-surge-protectors/forums/general/6096/apc-back-ups-rs-1100va-...] asking about this issue. i'd ask you to post any information you can provide into that thread so we can keep it all in one place. i am going to lock this thread.

but as i mentioned in the other post, we are aware of this issue now based on the posts you and some others have made in the past couple of days so we will be investigating and will post anything we get on the issue in the next week. please be patient since I understand it is annoying.

BillP
Administrator Administrator
Administrator
0 Likes
0
297

Re: Powerchute Personal Edition 3.0 - apcsystray.exe permissions startup bug

This reply was originally posted by Angela on APC forums on 9/7/2011


h1. this is now fixed!

PCPE version 3.0.0.1 is now available on the web. This is an interim release that is available in English & German and addresses three major concerns.

Fixes in this release:*

•With Windows UAC enabled, when a user logged on to Windows Vista or Windows 7, the UAC dialog always asked the user to approve starting the PowerChute Systray icon. This will no longer happen.

•After un-installing PowerChute, hibernation was not being restored and has been corrected.

• When selecting PowerChute Technical data screen it would be displayed very slowly and sometimes the internal PC fan made a lot of noise (indicating over usage). This has also been addressed.

Here is the link to the software or you can browse to it on apc.com/tools/download

http://www.apc.com/tools/download/software_comp.cfm?sw_sku=SFPCPE3001