Ask our Experts
Didn't find what you are looking for? Ask our experts!
Dear Community Members, We are currently experiencing a technical issue that is affecting the ability to create new posts. Our team is actively investigating the root cause and working to resolve it as quickly as possible. We apologize for the inconvenience and appreciate your patience. SE Community Team!
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Search in
Posted: 2021-06-28 02:15 AM . Last Modified: 2024-03-27 02:29 AM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-28 02:15 AM . Last Modified: 2024-03-27 02:29 AM
Ok so I bought this used ups APC RS 1500VA.
It was a bit charged so once home, I simply powered it on without connecting to mains. All seemed good on battery as on its back port/sockets I tried connecting my 3 phones for charging and then a basic Testing 250w psu with 6 led fans connected. And both the tests passed just fine!!!
Ok. Then I kept it for charging for 1h30mins and decided to test my system this time but only on ups backup battery mode.
My system specs:-
Phenom II X3 720BE @ stock
TA790GXA3+
Corsair XMS3 2*4 GB
XFX 9800GTX
Gigabyte Superb 460w
DELL S2240L
WD Blue 320GB
Hitachi 250GB
Samsung 80GB
Seagate 500GB
Seagate 500GB
Seagate 160GB
Creative 2.1 channel
Usb keyboard and mouse
******************************
Initially I connected my whole spikeguard directly to one of the ups back sockets/ports.(spikeguard had speakers/monitor/cpu/net modem) & it started and shut off within 5 secs. Shockingly!!
There wasnt any overload indication so I turned off ups and then just connected my spikeguard with only cpu and ips monitor this time and same thing happened.
What could be wrong?? The ups gives few beeps and only once it gave overload indication.
The Replace battery led doesnt glow so the battery wont be the issue.
UPS performs POST properly as mentioned in manuals.
Is it mandatory to keep the ups for charging for full charging before experimenting??? But the load of my system is just too low and I think it doesnt need full charging, just my thinking!
I checked my overall system power calculation on eXtreme Power Supply Calculatorand it comes down to only 380W.
Obviously now this UPS is 1500va i.e. 1500*60% = 900w So it should easily handle the 380w load. But it isnt doing so.
Also what do the ports Surge only stand for and what devices should be plugged in there?
In what ports shall I connect my spike guard to which will have only cpu/psu and ips monitor connected?
Or should I connect all the devices individually to UPS rather than using spike guard???
Now I have kept UPS for full overnight charging (8hrs is recommended for full battery charge) to test it tomorrow morning.
Fingers crossed....till tomorrow morning Dont know if my system will work on battery or not!!
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.