Just bought a BX1500LCD - Clarification please

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • Re: Just bought a BX1500LCD - Clarification please
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
Administrator BillP Administrator
2151
Teken
Kirk Teken
119
voidstar_apc
Janeway voidstar_apc
83
View All

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

0 Likes
3
1243
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
Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

Just bought a BX1500LCD - Clarification please

I haven't taken delivery yet, but I was told that on the back of the box there's an image of the back of the actual device with a map of the various plugs.

It shows what appears to be a 10/100 ethernet plug but it's labeled "Data Port to insure installation of DataChute software".

Can this UPS actually protect my network card or not?

This review at amazon http://www.amazon.com/review/R2G01UOVZEF3TR/ref=cm_cr_pr_viewpnt#R2G01UOVZEF3TR states the following

There are two models - BR1500LCD (Back UPS RS 1500) and BX1500LCD (Back UPS XS 1500). The difference:

*1. RS model has additional phone/fax/model/10/100base-T ethernet protection. The XS only has phone/fax/modem protection.*
*2. Auto Voltage Regulation is capable of BOOST (due from low voltage) and TRIM (from over voltage). Again, the XS model only has BOOST, and no TRIM feature.*

Can someone please clarify the actual differences? I had thought that the only difference was that the BX was retail and th BR was online.

Message was edited by: Kwyn

Labels
  • Labels:
  • Back-UPS & Surge Protectors
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

0 Likes
0
1243
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
Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

There is protection for phone and cable lines because they come in from outside the building, which makes them susceptible surges. LAN (cat5 etc) is inherently resistant to surges.

The RJ45 connector labeled "Data Port" is actually a USB port with a non-standard connector. My guess is that it's not labeled as a USB port because it doesn't conform to the USB standard. Any equipment that uses the term USB would have to conform to the USB standard, including connectors.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 3
Anonymous user
Not applicable

Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

0 Likes
0
1243
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
Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

I'm 99% sure I can explain the confusion, and if I'm wrong one of the APC guys can chime in...

The two jacks that you see for phone in/out are actually RJ-45 jacks which you can use to protect either a phone OR they will also accept a network patch cable. A standard phone cord (RJ-11) and network patch cable (RJ-45) will both fit in to this type of jack. But you can obviously only protect one device at a time.

The other RJ-45 jack below those is for the management cable, the cable has an RJ-45 connector on one end and a USB connector on the other, like in the attached picture file.

Regards,
Stew.

Attachments
Reply

Link copied. Please paste this link to share this article on your social media post.

Anonymous user
Not applicable

Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

0 Likes
0
1248
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
Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

Thank you

The unit was described to me as having an input for my dsl line which is a cat-5?

Seems odd to have 2 inputs for phone lines and none for internet cable

Reply

Link copied. Please paste this link to share this article on your social media post.

Anonymous user
Not applicable

Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

0 Likes
0
1244
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
Posted: ‎2021-06-29 12:03 AM . Last Modified: ‎2024-03-22 04:15 AM

There is protection for phone and cable lines because they come in from outside the building, which makes them susceptible surges. LAN (cat5 etc) is inherently resistant to surges.

The RJ45 connector labeled "Data Port" is actually a USB port with a non-standard connector. My guess is that it's not labeled as a USB port because it doesn't conform to the USB standard. Any equipment that uses the term USB would have to conform to the USB standard, including connectors.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.