Few question Back-UPS ES 550G --self-test--Overload Shutdown - Funny result
APC UPS for Home and Office Forum
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-2905:17 AM. Last Modified: 2024-03-2111:59 PM
Few question Back-UPS ES 550G --self-test--Overload Shutdown - Funny result
I have Back-UPS ES 550G
Firmware revision: 870.O2.I
Software version: PowerChute Personal Edition 2.0
It shows:
Result of last manual self-test is: Unsupported
And tehnical data:
Last manual self test date: Unsupported
*1.*what is this meaning?
-----
*2.*Do this model have Overload Shutdown?
[http://www.apcmedia.com/salestools/ASTE-6Z7V9M_R0_EN.pdf]
Says that there is Overload Shutdown, but who knows if it is automatic?
-----
*3*.Funny result, is this possible, did i miss something?
I get digital multimeter total load: 0.78A
0.78A x 230V = *183.3 VA*
And
This is what i get UPS Selector
-( Extra Power for future expansion value 0%)
-(AMD Athlon 64 2800+ is missing on list
i used AMD Athlon 64 2600+ )
Result:
APC Smart-UPS 1000VA LCD 230V
% of Max Capacity Used: 54 % = ( *540 VA* )