Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-06-2808:39 AM. Last Modified: 2024-03-2603:19 AM
Constant green light with noise UPS APC ES 550
Hi there,
I'm very old customer of APC UPS, having already about 4 different units. Here is the story of a very old version (over 10 years) of UPS APC ES 550 which was not used for years.
Battery is clearly dead and removed from Unit. I could use the UPS as surge only (only 4 outlets) without starting the UPS (not pressing the power button). On pressing the power button, i could use all outlets, but having the annoying noise and flashing led red. (perfect normal at this point)
So, i disabled the beep noise using PowerChute software, wanted to use ALL 8 outlets as surge protection only (or simple power multiplier). Unfortunately when reconnecting the unit on other power outlet, i got immediately the strange sound and constant green led on power button.
Really frustrating, a working unit (with that limitation on 4 outlets and no battery) after using PowerChute software to turn off beeping sound .. is now having a constant noise. Is basically unusable with such noise, although the 4 surge only outlets are still working.
May i know if this unit can still be used as power surge only ? Or at least simple power outlet multiplier. Can this noise be electrically (hardware) stopped ?
Trying to use PowerChute software doesn't work anymore, USB connection ( / or Unit) is not anymore recognized. I also tried "Reset the unit" but no luck (not sure if procedure was correct executed)