Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Best way to keep ups battery last longer?

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • Best way to keep ups battery last longer?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2151
Teken
Teken
154
Techie_apc
Techie_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2021-07-11 10:57 PM . Last Modified: ‎2024-03-19 11:44 PM

0 Likes
1
3641
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
Posted: ‎2021-07-11 10:57 PM . Last Modified: ‎2024-03-19 11:44 PM

Best way to keep ups battery last longer?

I recently purchase APC Back-ups pro 1000 to protect my PC. not going to use much of ups battery since i have home-ups as well. so i need to have battery last longer, so don't have to change battery anytime soon. 

wonder why its written warning 'do not switch off main power to the unit' on top of ups. i'd like to switch off main when i'm not using it. also is it better to turn main on for battery life or better off most of the time?

Labels
  • Labels:
  • Back-UPS & Surge Protectors
  • Tags:
  • apc
  • battery
  • ups
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Terry_Kennedy_apc
Terry_Kennedy_apc
Contributor

Posted: ‎2021-07-11 10:57 PM . Last Modified: ‎2024-03-19 11:44 PM

0 Likes
0
3641
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
Posted: ‎2021-07-11 10:57 PM . Last Modified: ‎2024-03-19 11:44 PM

In general, keep the batteries at a cool, constant temperature and avoid un-necessary discharge (for example, run-time calibration). Also, supply the appropriate float voltage, although that's not something you have control over - it is part of the UPS design. Depending on all of the above, you can generally expect a 2 to 5 year service life from SLA batteries. My rule-of-thumb (but this is for the more sophisticated Smart-UPS models) is one battery replacement, and then replace the whole UPS when it is time to replace those batteries. But that's just my opinion as an end user.

As far as warnings about input power, I'm not familiar with the particular model you're using. However, with the Smart-UPS models, the batteries are always powering the internal circuitry even when the UPS is "off". On models with a sensitivity LED on the rear panel, you can see that the UPS is still running even when off and unplugged. There is a procedure to "dead" the UPS - press and hold the off button with the UPS unplugged from the supply. You'll hear a click and the sensitivity LED will go out. There may still be some minor drain on the batteries, so if the UPS won't be used for a while, the battery disconnect (normally a plug on the back of the unit) should be activated - this is the reverse of the steps needed to connect things when the UPS is first installed.

Again, that's for Smart-UPS and above. I'm not sure if this applies to Back-UPS units. I'm sure one of the APC folks will correct me if needed. 

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
Terry_Kennedy_apc
Terry_Kennedy_apc
Contributor

Posted: ‎2021-07-11 10:57 PM . Last Modified: ‎2024-03-19 11:44 PM

0 Likes
0
3642
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
Posted: ‎2021-07-11 10:57 PM . Last Modified: ‎2024-03-19 11:44 PM

In general, keep the batteries at a cool, constant temperature and avoid un-necessary discharge (for example, run-time calibration). Also, supply the appropriate float voltage, although that's not something you have control over - it is part of the UPS design. Depending on all of the above, you can generally expect a 2 to 5 year service life from SLA batteries. My rule-of-thumb (but this is for the more sophisticated Smart-UPS models) is one battery replacement, and then replace the whole UPS when it is time to replace those batteries. But that's just my opinion as an end user.

As far as warnings about input power, I'm not familiar with the particular model you're using. However, with the Smart-UPS models, the batteries are always powering the internal circuitry even when the UPS is "off". On models with a sensitivity LED on the rear panel, you can see that the UPS is still running even when off and unplugged. There is a procedure to "dead" the UPS - press and hold the off button with the UPS unplugged from the supply. You'll hear a click and the sensitivity LED will go out. There may still be some minor drain on the batteries, so if the UPS won't be used for a while, the battery disconnect (normally a plug on the back of the unit) should be activated - this is the reverse of the steps needed to connect things when the UPS is first installed.

Again, that's for Smart-UPS and above. I'm not sure if this applies to Back-UPS units. I'm sure one of the APC folks will correct me if needed. 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.