Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84244members
353344posts

Battery life problem.

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
CloudSurfer_apc
Cadet
0 Likes
1
112

Battery life problem.

This was originally posted on APC forums on 5/17/2009


I live in Samoa where obtaining specific brands of new batteries is a logistic nightmare.

Three years ago I replaced my Smart UPS 1500 internal battery with two lead acid 35 AH 12 V batteries. I used heavy dutey wires, solder for joins and used the original fuse between the two batteries. This worked well and extended the battery run time modestly to about 45 mins. Recently, a problem has developed where it states that I have 5 min of battery time only. Assuming that the batteries had died, I went out and got two new ones, this time 40 AH, and connected them. The problem has remained. The computer drains about 17-20%.

I have tried to recalibrate but the system cancels this before it is completed. I have tried pulling the power plug and it only lasts a few minutes with the percentage charge dropping instantly from 100% to about 1% the moment it goes onto battery.

Clearly, it has worked previously with the external batteries and something new has happened.

UPS Model Smart-UPS 1500
Firmware Revision 601.1.I
Manufacture Date 28 June 2001
Serial Number AS0126231073

Tags (2)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
112

Re: Battery life problem.

This reply was originally posted by Angela on APC forums on 5/17/2009


okay so you arent getting the correct amount of runtime anymore as well as the software reporting the incorrect amount as well, correct?

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
113

Re: Battery life problem.

This reply was originally posted by Angela on APC forums on 5/17/2009


okay so you arent getting the correct amount of runtime anymore as well as the software reporting the incorrect amount as well, correct?