Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84724members
354137posts

Back-UPS Pro 650 Battery Swap - Can't budge the old battery this time

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
LC_apc
Cadet
0 Likes
1
76

Back-UPS Pro 650 Battery Swap - Can't budge the old battery this time

This was originally posted on APC forums on 10/25/2008


This is our 3rd battery swap. Great product but this time I can't budge the old battery. It rocks forward only every so slightly but won't move forward AT ALL. There is clearance on both sides but the ends seem tighter. I can even turn it upside down and I still can't budge the battery forward. Any ideas?

Tags (2)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
76

Re: Back-UPS Pro 650 Battery Swap - Can't budge the old battery this time

This reply was originally posted by Angela on APC forums on 10/26/2008


well, i'd personally recommend to think about trading the UPS in to APC/replacing the UPS.

the only reason i say that is because it is possible there is internal damage to the chassis that may impact the function of the UPS if you DO get the battery out. 😐

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
77

Re: Back-UPS Pro 650 Battery Swap - Can't budge the old battery this time

This reply was originally posted by Angela on APC forums on 10/26/2008


well, i'd personally recommend to think about trading the UPS in to APC/replacing the UPS.

the only reason i say that is because it is possible there is internal damage to the chassis that may impact the function of the UPS if you DO get the battery out. 😐