Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84702members
354081posts

BK650EI power consumption in off mode

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Glauco_apc
Crewman
Crewman
0 Likes
0
177

BK650EI power consumption in off mode

This was originally posted on APC forums on 3/4/2012


Hi there. I used to have two BK650MI connected to two pc’s of my LAN. Some weeks ago I realized by chance (losing my work) than one of this units was faulty (this old model doesn’t make a self test at start-up). It’s so that I substituted the faulty unit with a brand new BK650EI.

This new model is fine, however I was disappointed measuring that the power consumption in off/idle mode (i.e. when powered off, with nothing connected to the always-on line, and with the battery fully charged) has worsened to an average of 3.5W, while the old model has a dissipation of only 1.8W in this condition!

APC claims that the new models are more efficient that the old ones, perhaps this is true in battery mode, but, in all evidence, this is not true, at least for this unit, when it is in off/idle mode.

I strongly encourage APC engineers to pay attention to this aspect too in future designs.

As a turnaround to this problem, I will probably add a switch, to completely power off the unit, at least at night. Is there any reason not to do so?

Message was edited by: Glauco