Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84862members
354344posts

BE500U no light

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
W341_apc
Cadet
0 Likes
1
101

BE500U no light

This was originally posted on APC forums on 11/27/2011


This unit used to work fine, but last week it became dead, no light to power on/off, no output voltage at battery outlets, but surge protection outlets OK. Does it totally dead, or would some one please tell me the procedure to check it up?
Thanks.

w341
(This one was posted in General discussion)

Message was edited by: W341


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
102

Re: BE500U no light

This reply was originally posted by Jonathan on APC forums on 11/29/2011


Based from your description, it appears that you are having issues with the battery. There are three things that would commonly caused this and those are:

- Battery terminals are not properly connected
- Battery voltage is low
- Battery is too old

Let us start by making sure the terminals are properly seated and are not corroded. If you have a voltmeter, we could use that to measure if there's juice/sufficient voltage left on the UPS and also check if you have replaced the battery on this UPS before. If you have a spare battery that is compatible with this unit, we could swap them out.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
103

Re: BE500U no light

This reply was originally posted by Jonathan on APC forums on 11/29/2011


Based from your description, it appears that you are having issues with the battery. There are three things that would commonly caused this and those are:

- Battery terminals are not properly connected
- Battery voltage is low
- Battery is too old

Let us start by making sure the terminals are properly seated and are not corroded. If you have a voltmeter, we could use that to measure if there's juice/sufficient voltage left on the UPS and also check if you have replaced the battery on this UPS before. If you have a spare battery that is compatible with this unit, we could swap them out.