Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

APC Smart-UPS 1000VA + APC UPS Power Strip

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • APC Smart-UPS 1000VA + APC UPS Power Strip
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2150
Teken
Teken
150
voidstar_apc
voidstar_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2022-03-12 05:40 AM . Last Modified: ‎2022-03-12 05:40 AM

0 Likes
3
2302
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
Posted: ‎2022-03-12 05:40 AM . Last Modified: ‎2022-03-12 05:40 AM

APC Smart-UPS 1000VA + APC UPS Power Strip

I recently purchased APC Smart-UPS 1000VA which has 8 IC14 output connections. Since I use Type F AC outlet type I need IC14 to Type F adapter. The only APC product for that use I could find is APC UPS Power Strip PZ42I-GR which has 4 AC outlets type F and IC14 power plug connector. And the manual explicitly states;

1. A maximum of two UPS power strips can be installed per UPS. Only one can be used with each bank of battery

backup and surge outlets.
2. If a UPS does not have Surge Only outlets then only one UPS power strip is allowed.

Problem is I have 4 (out of eight outlets available. Since I didn't know about this rule I purchased 2 x APC UPS Power Strip PZ42I-GR. What would happen if I connect both so I can have 8 outlets? And is there another/better solution for this problem? Perhaps I can purchase some other non-APC product with 8 outlets?

Labels
  • Labels:
  • Back-UPS & Surge Protectors
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
APC_Matt
APC_Matt Contributor
Contributor

Posted: ‎2022-03-14 07:34 AM

0 Likes
1
2241
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
Posted: ‎2022-03-14 07:34 AM

Hi 

I think you will be ok you just need to make sure you aren't going to overload the output, we likely erred on the side of caution as it's easy to add extensions and keep plugging things in.

 

Looking at the assemble I don't see an issue plugging one adapter into an outlet on 1 side and 1 on the other side, it won't put any strain on the bus bars then that connect each of the sockets.

 

Regards

 

Matt

See Answer In Context

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 3
APC_Matt
APC_Matt Contributor
Contributor

Posted: ‎2022-03-14 07:34 AM

0 Likes
1
2242
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
Posted: ‎2022-03-14 07:34 AM

Hi 

I think you will be ok you just need to make sure you aren't going to overload the output, we likely erred on the side of caution as it's easy to add extensions and keep plugging things in.

 

Looking at the assemble I don't see an issue plugging one adapter into an outlet on 1 side and 1 on the other side, it won't put any strain on the bus bars then that connect each of the sockets.

 

Regards

 

Matt

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Anonymous user
Not applicable

Posted: ‎2022-03-14 03:57 PM

In response to APC_Matt
0 Likes
0
2228
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
Posted: ‎2022-03-14 03:57 PM

Hi, thanks for your answer! (is this "official" one?) I am far from output overload. Does this mean that theoretically I could plug another one (third one) as long as I am sure it will not going to overload the output? Just curious.

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

BillP
BillP Leader
Leader

Posted: ‎2022-03-16 08:25 AM

0 Likes
0
2185
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
Posted: ‎2022-03-16 08:25 AM

@Anonymous user 

 

You can connect two strips to the the UPS but you must be sure not to overload the UPS. And, you should balance the load between the outlet groups if you UPS has outlet groups.

 

On the SMT1000C there are two outlet groups. Group 1 and the Main. 

Back of SMT1000C.png

On the SMX1000 there are three outlet groups. 

Back of SMX1000.jpg

 

If the UPS does not have outlet groups balance the load with one strip per side. 

 

Back of SMC1000C.JPG
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.