Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84584members
353850posts

ACPSC2000 InRoom SC cooling unit.

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
lupeatx_apc
Crewman
Crewman
0 Likes
1
168

ACPSC2000 InRoom SC cooling unit.

This was originally posted on APC forums on 12/3/2012


I'm trying to set this is up in our server to work as a backup in case the main A/C goes out. I want to set it up to where if the server room temp gets to 75 degrees, this unit would turn on. I'm having trouble because unit stays on after setting the temp on it. At this time the server room is already at 70 degrees. Is there anything special that I need to do for it to turn off and not turn on until it has to.

Tags (2)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
168

Re: ACPSC2000 InRoom SC cooling unit.

This reply was originally posted by Angela on APC forums on 12/4/2012


The fan will always remain running in order to keep the sensor reading an accurate room temperature. The unit will also cool to a bit below the room temperature for the purposes of a hysteresis. However, if the unit is still cooling, try to make sure it is running in the "auto" mode. If it is and still doing this, try just the "cool" mode. The only other troubleshooting we can think of is trying a higher room temp, since it is possible the unit is seeing a higher room temp where it is located then where you are measuring.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
169

Re: ACPSC2000 InRoom SC cooling unit.

This reply was originally posted by Angela on APC forums on 12/4/2012


The fan will always remain running in order to keep the sensor reading an accurate room temperature. The unit will also cool to a bit below the room temperature for the purposes of a hysteresis. However, if the unit is still cooling, try to make sure it is running in the "auto" mode. If it is and still doing this, try just the "cool" mode. The only other troubleshooting we can think of is trying a higher room temp, since it is possible the unit is seeing a higher room temp where it is located then where you are measuring.