Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84468members
353684posts

725 VA, 450 Watts - Problems

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
deatsjoe_apc
Cadet
0 Likes
1
87

725 VA, 450 Watts - Problems

This was originally posted on APC forums on 6/29/2009


I've had this unit for a few years, and recently it had its first real test, in the form of a power outage. The computer remained on, until the battery ran out (I assume), and then it shut off.

This happened roughly a week ago. Since then, the UPS has randomly shut itself off about once a day. Its frustrating, because I'm never certain when its going to happen, and I'm not sure WHY it is happening.

There are no other signs of trouble from the UPS... certainly no beeping. Its relatively hidden from view, so I can't see any LED flashing.

Any suggestions?

Edit: And by 'shut itself off ', I mean that everything connected to the UPS loses power.

Message was edited by: deatsjoe


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
90

Re: 725 VA, 450 Watts - Problems

This reply was originally posted by Angela on APC forums on 6/29/2009


i am just throwing this out there but i have heard of a cat stepping n the power button or something like that. can we rule that out? it would be really helpful to see the LEDs also when it happens.

i cant say for sure whats happening, because it certainly isnt normal, but i cant really say much without knowing LEDs or anything else.

does it work correctly during a pull plug test? like plugging in a non critical load to the UPS and removing the AC power from the wall to see if it transfers to and from battery ok?

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
91

Re: 725 VA, 450 Watts - Problems

This reply was originally posted by Angela on APC forums on 6/29/2009


i am just throwing this out there but i have heard of a cat stepping n the power button or something like that. can we rule that out? it would be really helpful to see the LEDs also when it happens.

i cant say for sure whats happening, because it certainly isnt normal, but i cant really say much without knowing LEDs or anything else.

does it work correctly during a pull plug test? like plugging in a non critical load to the UPS and removing the AC power from the wall to see if it transfers to and from battery ok?