Posted: 2024-05-30 11:43 PM
Universal I/O port not working: 0N-1557
I am having difficulty installing a temp sensor into my SmartUPS-5000. Whenever I plug the sensor in (Universal I/O port 1), it will show connected, and then immediately afterwards it disconnects. I've rebooting the NMC, but it stays down. On the Web-GUI onder the Universal I/O status page, the only thing listed is under "Output Relay". It has "Port 1 Relay" listed in the "Lost comm" state. Not sure if that means anything, but I don't see that on my other UPS
5/10/2024 |
21:29:38 |
Device |
Environment: Lost the local network management interface-to-integrated Environmental Monitor (Universal I/O at Port 1) communication. |
0x0345 |
5/10/2024 |
21:29:38 |
Device |
Environment: Restored the local network management interface-to-integrated Environmental Monitor (Universal I/O at Port 1) communication. |
0x0344 |
5/10/2024 |
21:24:10 |
Device |
Environment: Lost the local network management interface-to-integrated Environmental Monitor (Universal I/O at Port 1) communication. |
0x0345 |
5/10/2024 |
21:24:10 |
Device |
Environment: Restored the local network management interface-to-integrated Environmental Monitor (Universal I/O at Port 1) communication. |
0x0344 |
This is my device and NMC information:
General
Model Number
0N-1557
Serial Number
xxxxxxxxxxxxxxx
Hardware Revision
3
APC OS (AOS)
Name
aos
Version
v2.0.0.6
Application Module
Name
su
Version
v2.0.0.5
APC Boot Monitor
Name
boot
Version
v1.4.0.2
Any help would be greatly appreciated
- Tags:
- english
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
Posted: 2024-05-31 06:51 AM
The NMC in the system is one of those embedded ones vs removable? Can you provide a picture of the back of the NMC and upload the same on the APC Forum.
Ensure the image is viewable on the forum.
Is the temperature sensor a AP9335T or AP9335TH temp / humidity sensor? Do you have another temperature sensor to check if the sensor is bad?
If you have another similar NMC in a UPS. What happens when you connect this specific temperature sensor into the other NMC?
Lastly, can you confirm what the NMC firmware is in both units.
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
Posted: 2024-06-02 01:54 AM
The NMC is the embedded kind (0N-1557 model). I don't have a pic of my device, but this one I got from Schneider looks exactly the same
I'm using the AP9335TH temp sensor. I have another Smart-UPS-5000 in another cabinet, and I've tested the sensor in that one, so I know it works. When it connects, it will show under the "Temperature & Humidity" header on the "Universal I/O" tab. I've also tried a brand new sensor, with the same results
I'm not 100% sure how I can check the firmware on the NMC (unless its in the information I've posted, AOS, Application Module, etc.). There is this, but I think its the UPS firmware not the NMC
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
Posted: 2024-06-03 03:58 AM
RE: NMC firmware, just wanted to see if both units were on the same firmware as you posted up above (AOS / App). If you haven’t done so already I would consider three options from least invasive to the most invasive from:
Default the NMC via the internal web browser.
Firmware: Reload the same NMC firmware.
Format: This will erase all settings and reset the NMC to an OEM state.
Link copied. Please paste this link to share this article on your social media post.