Posted: 2022-10-14 02:03 AM
Serial communications for SRT3000RMXLI
Hi all,
Have been trying to log in through CLI to capture logs of UPS through serial port using USB to serial ( APC rj45 cable provided).
I had success in connecting and upgrading firmware with the wizard.
CLI seems to be connecting but not showing anything even upon pressing enter a few times.
Model of UPS is SRT3000RMXLI
Programs used: hypertrm, teraterm, putty
Settings:
Baud rate:2400,4800,9600,19200
Data bits: 8
Parity: None
Stop bits: 1
Flow control: None
Appreciate anyone who could help. Thanks!
Link copied. Please paste this link to share this article on your social media post.
Accepted Solutions
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
Posted: 2022-10-17 10:51 PM
Since this UPS has an LCD, the last ten faults and events can be retrieved from the display. Unfortunately, accessing the network card or installing PowerChute Business Edition on a supported OS will let you know more about the UPS and will provide more logging features.
- Tags:
- english
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
Posted: 2022-10-16 03:12 PM
Hi @RMAmeerul
Thank you for reaching out to the SE Community, my name is Jon and I will assist you with this query.
By any chance, is there a network management card installed on the UPS? The reason I asked is that, if you'd like to communicate to the UPS via the CLI, it needs to have a network management card, and for you to connect to the card using the supplied cable.
- Tags:
- english
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
Posted: 2022-10-16 07:32 PM
HI @JonPro
Thanks for the reply,
There is a network card installed on site, which we are unable to retrieve to test due to sensitivity and I understand this part on connecting to CLI through NMC.
I think my real question would be whether the UPS saves logs internally and whether am I able to retrieve it using any of the port that is installed on the UPS itself? Eg. Rj45 serial port (used for firmware upgrade) or USB port.
Thanks!
- Tags:
- english
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
Posted: 2022-10-17 10:51 PM
Since this UPS has an LCD, the last ten faults and events can be retrieved from the display. Unfortunately, accessing the network card or installing PowerChute Business Edition on a supported OS will let you know more about the UPS and will provide more logging features.
- Tags:
- english