Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-2805:14 AM. Last Modified: 2024-03-1803:41 AM
SURTD2200XLIM Can`t connect with hyperterminal
Hello,
We have a SURTD2200XLIM, It`s a new unit with 2 extra battery packs which I need to add in the UPS configuration (we installed a AP9613 unit in the UPS).
The unit has a RJ45 serial com connection and I use the 940-1525A communication cable that was delivered with the unit.
We tried bps 2400 and 9600 both with 8 data bits, parity none, stop bit 1, flow control none. Tried with 3 different laptops, one with USB to DB9 (others directly on DB9 on laptop), tested programs Hyperterminal and ADRCOM. Also tried braindeading the UPS to reset communications without luck.
On 1 laptop powerchute laptop is installed, UPS can communicate with server.
In Hyperterminal the screen remains blanck when the correct com port is selected (when wrong port is selected I see the commands I type).