SURT10000XLi Connection

APC UPS Data Center & Enterprise Solutions Forum

Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
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
  • SURT10000XLi Connection
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
139
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
Not applicable

Posted: ‎2021-06-29 06:29 AM . Last Modified: ‎2024-03-12 11:28 PM

0 Likes
1
1495
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
Posted: ‎2021-06-29 06:29 AM . Last Modified: ‎2024-03-12 11:28 PM

SURT10000XLi Connection

Hello,

I have just installed an APC UPS and I am unable to connect to it to configure the Powerchute software. I have plugged in a serial cable and put in the settings that are listed in the UPS manual, but it doesn't connect. Does anyone have a suggestion of how I can configure it with an IP address to I can try to connect via a web page? I am getting nowhere with the Serial connection.

I have used the following settings from the user guide:

Start

=> Programs

=>

Accessories

=> Communication

=>

HyperTerminal.

2
. Double-click on the
HyperTerminal

icon.




Follow the prompts to choose a name and select an icon. Disregard the message, "...must install a modem," if it is displayed. Click OK.
Select the

COM1

port that is connected to your UPS. The port settings are:
bits per second - 2400
data - bits 8
parity - none
stop bit - 1
flow control - none

When I do this I just get a blank screen. I was expecting to be prompted with a username and password?

Can anyone help?

Cheers




Labels
  • Labels:
  • Smart-UPS & Symmetra LX | RM
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
Administrator

Posted: ‎2021-06-29 06:30 AM . Last Modified: ‎2024-03-12 11:28 PM

0 Likes
0
1495
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
Posted: ‎2021-06-29 06:30 AM . Last Modified: ‎2024-03-12 11:28 PM

You do not use HyperTerminal to configure PowerChute. PowerChute is installed and configured on the computer system.

If you are attempting to configure a network management card that is installed on the SURT then when you get to the blank screen you should press enter a few times and then you will be asked for the user name and password. The setting you listed above are correct if the network card is model AP9617, AP9618, or AP9619. If the network card is model AP9630 or AP9631 then the bits per second should be 9600. In order to connect to one of these cards, you should use the 940-0299 Tip, Ring Sleeve (TRS) to DB9 cable and connect it directly to the NMC2 into the 2.5mm jack labeled "console" rather than the UPS serial port.

  • Within a UPS, the NMC2 devices communicate with the following port settings:

             9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control.

  • Apply the port settings to establish the connection.
  • Press enter 3-5 times to display the username prompt.
  • Use the default username and password of  "apc"


See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-29 06:30 AM . Last Modified: ‎2024-03-12 11:28 PM

0 Likes
0
1496
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
Posted: ‎2021-06-29 06:30 AM . Last Modified: ‎2024-03-12 11:28 PM

You do not use HyperTerminal to configure PowerChute. PowerChute is installed and configured on the computer system.

If you are attempting to configure a network management card that is installed on the SURT then when you get to the blank screen you should press enter a few times and then you will be asked for the user name and password. The setting you listed above are correct if the network card is model AP9617, AP9618, or AP9619. If the network card is model AP9630 or AP9631 then the bits per second should be 9600. In order to connect to one of these cards, you should use the 940-0299 Tip, Ring Sleeve (TRS) to DB9 cable and connect it directly to the NMC2 into the 2.5mm jack labeled "console" rather than the UPS serial port.

  • Within a UPS, the NMC2 devices communicate with the following port settings:

             9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control.

  • Apply the port settings to establish the connection.
  • Press enter 3-5 times to display the username prompt.
  • Use the default username and password of  "apc"
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.