Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-06-1507:20 AM
SMX3000HV firmware update issues
Hi All,
I just got a used APC SMX3000HV (no network card). It came with the 7.4 firmware and I am trying to update it to the latest firmware (15.0, it seems) using the firmware update wizard (v4.3.8).
I'm running the firmware update wizard using an USB cable from a Windows 10 Lenovo Laptop.
When I launch the firmware update wizard, it finds the UPS and properly determines that the firmware needs to be upgraded from 7.4.
Then, I follow the various prompts, select the firmware file and the UPS starts displaying 'Firmware update in progress'. Then, after just a few seconds, the UPS powers down hard (See video below) and the Upgrade Wizard on the Windows machine is stuck at: "sending device firmware file 1 of 1 : 6%"
I waited over 10 minutes but nothing else happened. After that delay, I pressed briefly the large power button on the UPS and it came back, still on firmware 7.4.
Does anyone have any tips? How do I flash the firmware update? Must I use a serial cable? (any links to amazon cables would be helpful if that is so).
After 2 hours (yes, hours), the progress bar had moved from 6% to 10%. Should I try a serial connection instead for the firmware update?
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-11-3005:56 AM
Having the same issue with the same model and software combo.
in the FUW_readme.txt it does say that updating this model over USB is not supported in that revision of the software but, doing this over serial is not working either.
I have tried using a few serial cables through serial to USB adapters(DB9), but the firmware upgrade software never connects just attempts to connect and then fails.
trying to connect over putty doesn't seem to work either.
did you end up getting any support for this @ElCoyote777 ?