Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84248members
353347posts

How do I get PowerChute 9.0 (Build 613) to send an email on restart?

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
QuietLeni_apc
Cadet
0 Likes
1
174

How do I get PowerChute 9.0 (Build 613) to send an email on restart?

This was originally posted on APC forums on 2/16/2012


Dear All,

I am working with PowerChute 9 and I have got the software to email to me when the server goes down, but it does not email when it comes back up.

I have had it working when working in another company and it worked out-of-the-box, but this time, there is no email, so, i get two emails (one for power failure and one for going down), but nothing to tell me the thing is back up! I used to get the third email as well.

Are there any logs I can go to for this?

Kindest regards,

QuietLeni

Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
174

Re: How do I get PowerChute 9.0 (Build 613) to send an email on restart?

This reply was originally posted by Chris on APC forums on 2/17/2012


If you log into the agent directly, you can see all the UPS settings including notifications. Under events, then actions, you can see all the available events. The closest i could find for you that might help is communication established or power restored. You can click on each one and edit the options such as enabling email. The agent interface can be accessed from the start menu under the APC folder(may be labeled as APC or powerchute business edition) The link below may also work if the agent is installed on the computer you are accessing it from.

https:\\127.0.0.1:6547

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
175

Re: How do I get PowerChute 9.0 (Build 613) to send an email on restart?

This reply was originally posted by Chris on APC forums on 2/17/2012


If you log into the agent directly, you can see all the UPS settings including notifications. Under events, then actions, you can see all the available events. The closest i could find for you that might help is communication established or power restored. You can click on each one and edit the options such as enabling email. The agent interface can be accessed from the start menu under the APC folder(may be labeled as APC or powerchute business edition) The link below may also work if the agent is installed on the computer you are accessing it from.

https:\\127.0.0.1:6547