High Earth voltage at Smart UPS Output on battery operation

APC UPS Data Center & Enterprise Solutions Forum

Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
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
  • High Earth voltage at Smart UPS Output on battery operation
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
139
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
Not applicable

Posted: ‎2021-06-29 08:15 AM . Last Modified: ‎2024-03-12 03:11 AM

0 Likes
1
3099
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
Posted: ‎2021-06-29 08:15 AM . Last Modified: ‎2024-03-12 03:11 AM

High Earth voltage at Smart UPS Output on battery operation

I understand after reading APC support (FAQ FA156549) but is it possibel to to reduce the output Earth voltage(Between Netral to Earth) for client satisfaction after doing some hardware changes with Earth, Netral or Using separate Earth or some component network?

Mukhtar

Labels
  • Labels:
  • Smart-UPS & Symmetra LX | RM
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
Administrator

Posted: ‎2021-06-29 08:15 AM . Last Modified: ‎2024-03-12 03:11 AM

0 Likes
0
3097
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
Posted: ‎2021-06-29 08:15 AM . Last Modified: ‎2024-03-12 03:11 AM

While "On Battery," safety agencies (UL, VDE, etc.) require the UPS input connections to be disconnected from the utility input to prevent "backfeed" power/voltage from the UPS batteries being applied to the UPS input terminals. Because the Neutral must also include this "backfeed" protection (we do it by opening a relay), the output Neutral to Ground voltage will "float" to approx half the voltage between output Line & Neutral. For a 230Vac system, the N-GND voltage can be 115Vac.  This does not become a safety hazard because the output L & N conductors are not user-accessible.  They are both always considered "high voltage" conductors.

If the UPS output must have a N-GND connection for zero volts while the UPS is "On Battery," an output isolation transformer must be attached to the UPS output so that a new N-GND connection can be made without creating a ground loop. We sell isolation transformers that can be used for this, if required.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-29 08:15 AM . Last Modified: ‎2024-03-12 03:11 AM

0 Likes
0
3098
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
Posted: ‎2021-06-29 08:15 AM . Last Modified: ‎2024-03-12 03:11 AM

While "On Battery," safety agencies (UL, VDE, etc.) require the UPS input connections to be disconnected from the utility input to prevent "backfeed" power/voltage from the UPS batteries being applied to the UPS input terminals. Because the Neutral must also include this "backfeed" protection (we do it by opening a relay), the output Neutral to Ground voltage will "float" to approx half the voltage between output Line & Neutral. For a 230Vac system, the N-GND voltage can be 115Vac.  This does not become a safety hazard because the output L & N conductors are not user-accessible.  They are both always considered "high voltage" conductors.

If the UPS output must have a N-GND connection for zero volts while the UPS is "On Battery," an output isolation transformer must be attached to the UPS output so that a new N-GND connection can be made without creating a ground loop. We sell isolation transformers that can be used for this, if required.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.