Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84449members
353655posts

Connect HP 252663-D75 Modular Power DIstrobution Units to Symmetra LX?

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
gdanieli_apc
Cadet
0 Likes
1
152

Connect HP 252663-D75 Modular Power DIstrobution Units to Symmetra LX?

This was originally posted on APC forums on 8/3/2007


How do I connect an HP c7000 blade enclosure to a Symmetra LX 16kVA unit?

I have 2 x HP 40A Core Modular Power Distribution Unit 252663-D75 units that must be connected to the Symmetra.

Thanks!


Accepted Solutions
Grenade_apc
Lieutenant
Lieutenant
0 Likes
0
152

Re: Connect HP 252663-D75 Modular Power DIstrobution Units to Symmetra LX?

This was originally posted on APC forums on 8/3/2007


From looking at HP's site this distribution unit's input requirements are: Input: 3.6m Attached Input cord, Non-NEMA Locking CS8265C, 50A. APC does not have any type of receptacle for this plug. You would either need to swap the input plug on the power distribution units to something smaller like a 30 amp plug, ie L6-30. Doing this would in turn downgrade the capacity of the PDU's to 30 amps vs. the 50 amps the device appears to be capable of pulling. I think the best option would be to have someone hardwire the output of the UPS to accomodate for the CS8265C plugs. An electrician can create a distribution panel with whichever outlets you desire to connect other devices as well. This would allow you to take advantage of the full capacity of your PDU's.

See Answer In Context

1 Reply 1
Grenade_apc
Lieutenant
Lieutenant
0 Likes
0
153

Re: Connect HP 252663-D75 Modular Power DIstrobution Units to Symmetra LX?

This was originally posted on APC forums on 8/3/2007


From looking at HP's site this distribution unit's input requirements are: Input: 3.6m Attached Input cord, Non-NEMA Locking CS8265C, 50A. APC does not have any type of receptacle for this plug. You would either need to swap the input plug on the power distribution units to something smaller like a 30 amp plug, ie L6-30. Doing this would in turn downgrade the capacity of the PDU's to 30 amps vs. the 50 amps the device appears to be capable of pulling. I think the best option would be to have someone hardwire the output of the UPS to accomodate for the CS8265C plugs. An electrician can create a distribution panel with whichever outlets you desire to connect other devices as well. This would allow you to take advantage of the full capacity of your PDU's.