Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Communication lost Smart-UPS 1000

APC UPS Data Center & Enterprise Solutions Forum

Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS Data Center & Enterprise Solutions Forum
  • Communication lost Smart-UPS 1000
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
Administrator BillP Administrator
5059
voidstar_apc
Janeway voidstar_apc
196
Teken
Kirk Teken
146
View All

Recommended Forums

  • APC UPS for Home and Office Forum

  • EcoStruxure IT Forum

Free

English

Data Center Certified Associate Exam Development Path

Strengthen your foundational knowledge in Data Centers for free, enroll in this path today and start your learning journey!

4.0
Register Browse SE University

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to APC UPS Data Center & Enterprise Solutions Forum
Start a Topic
Smartuser
Smartuser
Cadet

Posted: ‎2024-11-07 10:34 PM

0 Likes
1
704
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
Posted: ‎2024-11-07 10:34 PM

Communication lost Smart-UPS 1000

Hello,

How it works connecting UPS to smart connect ?

I added 5 devices, but i have status "Communications Lost"

I understand that when added to the application, the devices are visible, but once connected, communication is lost?

Devices had static IP address.

DNS are requirement?

Who sending signal about connection- UPS or smart connect?

 

Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
RyanG32
Ensign RyanG32 Ensign
Ensign

Posted: ‎2024-11-10 12:30 PM

0 Likes
0
661
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
Posted: ‎2024-11-10 12:30 PM

Please check smartconnect status depending on the status there will be different troubleshooting

 

Go to the Configuration menu of the UPS and make sure that smart connect is enabled then try to reset the connection

 

UPS models with the prefix SMX, SMT including Lithium ion
To reset the network interface of an SMX/SMT model UPS, on the display interface, hold the UP and DOWN buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted.
 
UPS models with the prefix SMC
To reset the network interface of an SMC model UPS, on the display interface, hold the MUTE and MENU buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted.
 UPS models with the prefix SCL

RyanG32_1-1731270297917.png


To reset the network interface of an SCL model UPS, insert a paperclip in the reset hole in the rear of the UPS.


Check where the unit status stops if changes to Connected the unit should be good

 

 

Network Requirements
If your SmartConnect-compatible UPS is installed in an enterprise location, it may require additional network configuration to allow your UPS to connect to Schneider Electric cloud services.

IPv4 DHCP Server
A SmartConnect device requires an IPv4 DHCP server on its network to assign an IPv4 address to the device so it can connect to the Internet.

Network MTU
The router and switch on the network of the SmartConnect device must support a Maximum Transmission Unit (MTU) size of 336 bytes at a minimum.

 Network Firewall and Proxy Server

NOTE: When a user wants to connect their UPS to Ecostruxure, it must be connected to the SmartConnect cloud portal, so the network settings listed below are the same. The only difference is they would not add the UPS to a SmartConnect account. They would add the UPS to Ecostruxure. 

 

  • To connect to Schneider Electric cloud services, the UPS must connect directly to TCP port 443 on cece.prod.struxurewarecloud.com (20.121.83.246). If the UPS network is behind a proxy server (e.g., ZScaler), you must add a firewall rule that permits this connection to TCP port 443 and bypasses any proxy service packet inspection. Consult with your Network Administrator to configure this firewall rule.

Please make sure that you have the latest firmware f the UPS just in case it connects to an old server

 

APC recently migrated devices from the cloud server URL (lwm2m.na.struxurewarecloud.com) to the new system URL (cece.prod.struxurewarecloud.com). The system will run in parallel until the migration is complete so that we will remove the old server URL in time.

 New Network Firewall and Proxy Server

  • To connect to Schneider Electric cloud services, the UPS must connect directly to TCP port 443 on cece.prod.struxurewarecloud.com AND lwm2m.na.struxurewarecloud.com.

Switch port speed:
SmartConnect-compatible UPS devices only support 10/100 Mbps port speed. If you are using a 1Gb network switch, and the port is not set to auto-configure its speed, this can prevent the device from connecting to Schneider Electric cloud services.

 

SMC status indicators
The SmartConnect status is located under the STATUS menu and is reached by pressing the MENU button until the SmartConnect status is displayed.  The tables below show the values listed.
 

State Description Type -3
7-Segment Display
1 Connecting to host UPS n/a
2 FW Updating Host UPS n/a
3 Obtaining Local IP Address (DHCP) Sc.2
4 Resolving cloud address (DNS) Sc.3
5 Connection being Established Sc.4
6 Securing the connection (TLS) Sc.5
7 Communication Starting Sc.6
8 SmartConnect Connected Sc.1
     
11 No Ethernet connection Sc.0
12 No Internet connection  
13 Ethernet prohibited Sc.8
14 Ethernet Disabled Sc.7

 


SMT, SMX, and SRT status indicators
The SmartConnect status is located under the STATUS menu and is titled "SmartConnect:" The table below shows the value listed under the status for various conditions.
 

State Description SmartConnect
Status
     
     
3 Obtaining Local IP Address (DHCP) Addressing
4 Resolving cloud address (DNS) Addressed
5 Connection being Established Resolved
6 Securing the connection (TLS) Attempting to connect to
the cloud
7 Communication Starting Secured
8 SmartConnect Connected Connected
     
11 No Ethernet connection No Ethernet
12 No Internet connection No Internet
13 Ethernet prohibited Prohibited
14 Ethernet Disabled Disabled
     
     

 

 

Run a Wireshark capture and check the communications between UPS and the cloud. To run the capture connect a PC to the same network as the UPS and launch Wireshark. Press and host the UP and down arrows of the UPS for 10 seconds to reset communications. The UPS will attempt to connect to the cloud.

Below is an example of a good connection.

 

 

The UPS is IP address 192.168.0.156. The cloud is 20.121.83.246 (domain name cece.prod.struxurewarecloud.com)

The UPS sends a TCP packet, and the cloud replies. Then the UPS sends a TLS packet "Client Hello," and the cloud replies with TLS "Server Hello."

If they do not see the reply "Server Hello" the local network is dropping the packet and the connection will fail.

 

 

RyanG32_2-1731269913735.png
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.