Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84589members
353854posts

AP8659 Firmware Download Issue

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

ericmcd81
Cadet
0 Likes
5
505

AP8659 Firmware Download Issue

I have an APC AP 8659 PDU with an apparently corrupted rpdug2 application on it (the app status is A-). The bootmon and AOS look to be good based on the status when I ssh into the unit. The Firmware version appears to be at 6.8.0 (AOS 6.8.2, Bootmon 1.0.9), so I went to the website to try to download 6.8.0, but every 6.8.0 page has embedded links back to 6.5.6 which is frankly infuriating. I also can't seem to access the APC FTP site to check and see if I can find it there. Would someone be able to provide me a link to 6.8.0, or baring that, is it possible to downgrade the whole unit (bootmon, AOS and APP) back to 6.5.6. Thank you all for your time.

Tags (1)
5 Replies 5
JohnBT
Ensign Ensign
Ensign

Re: AP8659 Firmware Download Issue

Hello,

 

I sent you a DM to download FW 6.8.0.  I will also include FW 7.0.4 which is the latest.

 

 

Tags (1)
AndreasG
Crewman
Crewman
0 Likes
3
410

Re: AP8659 Firmware Download Issue

Same issue with trying to download the latest and greatest firmware for AP8659. They run on OS 6.8.2 (App 6.8.0) and because of some SNMP hicups I was looking for fresh firmware for the maintenance window... but.. am I doing something wrong? Why isn't it listed anywhere? Reasons I've missed? So weird. 7.0.4 is out as well... where did you find that? Cheers!

Tags (3)
JonPro
Lt. Commander Lt. Commander
Lt. Commander

Re: AP8659 Firmware Download Issue

Hello @AndreasG,

 

I have sent you a DM that has the link to where you can download the v7.0.4 PDU firmware.

Regards,

JonPro
Secure Power Team
Tags (1)
systeembeheer_apc
Crewman
Crewman
0 Likes
1
173

Re: AP8659 Firmware Download Issue

Hi we are running on software version 6.7.2 wanted to download a new firmware version but cannot find it anywhere on the Schneider site. Any help please?

Tags (1)
JohnBT
Ensign Ensign
Ensign
0 Likes
0
159

Re: AP8659 Firmware Download Issue

Hello,

 

I sent you a DM where you can download the latest firmware.

 

Cheers,

 

Tags (1)