• About Rajeev_211
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Rajeev_211
Rajeev_211
Crewman
‎2025-08-11
4
Posts
0
Likes Received
3
Likes Given
0
Solutions

Community Badges

Open Hailing Frequencies
Resistance is Futile
There's coffee in that nebula.
Let's see what's out there.
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Rajeev_211
/html/rank_icons/Crewman.png Rajeev_211 /html/rank_icons/SE-Employee.png

Saitel DR - Can one have more than one Modbus Master connected to HUe?

I have made one modbus TCP slave PHG66301A in saitel HUe, when I am checking the modbus slave data on modbus poll master, its working and reading the ...
EcoStruxure Power & Grid icon_circle Protection & Control
341 0 2

2025-08-10 09:09 PM

Rajeev_211
/html/rank_icons/Crewman.png Rajeev_211 /html/rank_icons/SE-Employee.png

Easergy Builder - In CoreDB, how to configure Modbus slave device's SP...

Hi,I have to add a modbus slave device SPC (single point command) command having register address 1 (holding) HR bit 6 in Saitel HUe easergy builder ...
EcoStruxure Power & Grid icon_circle Protection & Control
607 0 5

2025-07-08 07:33 PM

Activity Feed
  • Posted Saitel DR - Can one have more than one Modbus Master connected to HUe? on Protection & Control. ‎2025-08-10 09:09 PM
  • Tagged Saitel DR - Can one have more than one Modbus Master connected to HUe? on Protection & Control. ‎2025-08-10 09:09 PM
  • Liked Re: Easergy Builder - In CoreDB, how to configure Modbus slave device's SPC command into bits (.i.e., HR 1 having bit 6 for SPC command)? for JuanRayo. ‎2025-07-14 05:37 PM
  • Posted Re: Easergy Builder - In CoreDB, how to configure Modbus slave device's SPC command into bits (.i.e., HR 1 having bit 6 for SPC command)? on Protection & Control. ‎2025-07-09 06:23 PM
  • Liked Re: Easergy Builder - In CoreDB, how to configure Modbus slave device's SPC command into bits (.i.e., HR 1 having bit 6 for SPC command)? for JuanRayo. ‎2025-07-09 06:17 PM
  • Posted Re: How to configure Modbus slave device SPC command in core DB of easergy builder for whose command is in bits..i.e. HR 1 having bit 6 for SPC comman on Protection & Control. ‎2025-07-09 12:05 AM
  • Posted Easergy Builder - In CoreDB, how to configure Modbus slave device's SPC command into bits (.i.e., HR 1 having bit 6 for SPC command)? on Protection & Control. ‎2025-07-08 07:33 PM
  • Tagged Easergy Builder - In CoreDB, how to configure Modbus slave device's SPC command into bits (.i.e., HR 1 having bit 6 for SPC command)? on Protection & Control. ‎2025-07-08 07:33 PM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.