Voice Control for Wiser for KNX - New update, fixing issues with blinds and shutters
We're glad to communicate that yesterday we have released a small update in the Voice Control service for both Alexa and Google fixing the direction in which the shutters and blinds move, making it consistent with the commands used.
This change means that the values (%) used for moving the blinds are now inverted as shown in the table below. This is important to keep in mind because it means a change for everyone who controls the blinds by setting a percentage.
|
Before |
Now |
Blind completely opened |
0% |
100% |
Blind 1/4 opened |
25% |
75% |
Blind 3/4 opened |
75% |
25% |
Blind completely closed |
100% |
0% |
For example: To close just ¼ of the blind, the blind was previously set to 25%; now, the blind needs to be set to 75% instead (as otherwise, 25% will now bring the blind to 3/4 the height)
Moving the blinds Up or Down through Voice control will now work literally according to the supported commands in both Systems:
Alexa: "Blinds up/down", "Increase/decrease blinds", "Make blinds darker/brighter", "Roll blinds down/up", "set the blinds to X", etc.
Google: "Close/Open blinds" , "Open/close the blinds to x%"
Thanks
Your Wiser for KNX team
- Labels:
-
Information
-
Local App
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
Ok, What about Homekit Apple support.
Most of our "rich" customer use Apple not google or alexa