HI,
Fairly new to the SpaceLYnk so apologies if this is a silly question but I can't seem to find the answer.
What is the Default Network ID on the SpaceLynk and is it possible to change this to a new number. I can see where the Device ID can be changed but not the Network ID.
Thanks
- Labels:
-
SpaceLYnk
Authentication Failed.
- Authentication Ticket Mismatched, failed authentication.
Accepted Solutions
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
Hi AndyRolly,
BACnet network numbers are assigned within BACnet router.
spaceLYnk is not a router, so this isn’t a property on this device.
Thomas
Application Design Engineer
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
In Niagara this is known as the Network number. It can be between 1 and 65,534.
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
Thank you - that makes sense as the Jace is.