Problem with the control of the Haier air conditioning system
SpaceLogic KNX Forum
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2024-12-2404:09 AM
Problem with the control of the Haier air conditioning system
Has anyone encountered a similar problem?
I have a problem with the control of a Haier air conditioning system. This system is controlled using the SpaceLYnk controller and the YCJ-A002 adapter (Haier) via the Modbus RTU protocol and also separately from another wired remote control. The problem is that when controlling the air conditioner from the remote control, no state change is registered in the SpaceLYnk controller. That is, if you turn on the air conditioner from the remote control (“ON/1” mode), the register of the YCJ-A002 adapter (Haier) responsible for the state of the air conditioner changes, but in the SpaceLYnk controller it remains in “OFF/0” mode.
I also attach a file with Modbus mapping for the YCJ-A002 adapter (Haier) for a more complete picture.