Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2022-05-3007:23 AM
Multitouch Pro with Floor Heating (KNX)
Hallo everyone,
I have a KNX system with MultiTouch pro as Thermostat in each room (MTN6215-5910), an underfloor Remote Sensor (MTN5775-0003), and an underfloor heating system with its valve connected to Switch Actuator.
The MultiTouch Pro is configured as a Heating type of control, PI-Control underfloor heating with no additional level, the output of Pi control is PI Control (switching), with no fan.
My problem is: The multitouch pro keeps the valve on when though setpoint of temp is 17 and room temp is 24.
could anyone help what is the problem here? I used an object (Correcting variable heating (basic level)) to control the system (it is in one group address with a valve (switch actuator) is it the right method?