SpaceLogic KNX Forum
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Link copied. Please paste this link to share this article on your social media post.
ANY BODY KNOWS IF THE LSS100400 IS COMPATIBLE WITH POWERTAG METER SENSORS.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hi
As Erwin already stated, the Hybrid module is not compatible with Schneider wireless powertags; however, we have recently launched a new Wired Powertag that connects to the Wiser for KNX/spaceLYnk controllers through Modubus. It is a great option, also from the price point of view. This device is currently available as a 1 phase meter and it has been released in a few European countries, and will later be rolled out to others but the 3-phase is coming later this year.
https://www.se.com/de/de/download/document/R9M80X6M_SW/
Thanks
Fernando
Link copied. Please paste this link to share this article on your social media post.
Fernando thanks that's a great solution.
Link copied. Please paste this link to share this article on your social media post.
And if wireless is preferred, you can use a PAS400 for connecting the Powertags and read them vIa the panel server over Modbus TCP.
Link copied. Please paste this link to share this article on your social media post.
You can also use the TCP modbus comunication with this R9M80X6M using an adapter with this specifications, for example:
ELFIN-EE11A - Ethernet - http://www.hi-flying.com/index.php?route=product/product/show&product_id=247
ELFIN-EW11A - Wifi - http://www.hi-flying.com/elfin-ew10-elfin-ew11
Link copied. Please paste this link to share this article on your social media post.
Hi,
just bought the new LS100400, in the belif that it would suport the schneider powertags, zigbee lights, elko devices and so on.
It is so frustrating with all the scheider devices that is not supported over the different platforms/gateways!
First I bought the Powertag link, --> Integrated with WISER KNX, but it apears that this can not use 3 pole Acti9 powertag (1 pole/ 2 pole/ 4 pole OK) ( And of course this product is not supported any more)
--> Finally I thought I had found the ONE device/ gateway that could replace Philipps Hue bridge, USB zigbee (ebay), & PowertagLink.....
So from my opinion there should be limits to what you SE guys should exspect customers and user to buy of devices over and over again, also from a enviromental perspective.
it`s so frustrating and disapointing!
BR
GIA
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.