Hello,
I have noticed following activity on my Homelynk... Is this some normal activity? Firmware V1.5.1
Is this related to the Schneider VPN application or is thi shecking activity ?
establish TCP connection with [AF_INET]40.118.18.71:443 [nonblock]
Aug 28 19:58:56 homeLYnk daemon.notice openvpn[917]: SIGUSR1[soft,auth-failure] received, process restarting
Aug 28 19:58:56 homeLYnk daemon.notice openvpn[917]: AUTH: Received control message: AUTH_FAILED
Aug 28 19:58:53 homeLYnk daemon.notice openvpn[917]: [serverSouth] Peer Connection Initiated with [AF_INET]40.118.18.71:443
Aug 28 19:58:51 homeLYnk daemon.notice openvpn[917]: TCPv4_CLIENT link remote: [AF_INET]40.118.18.71:443
Aug 28 19:58:51 homeLYnk daemon.notice openvpn[917]: TCPv4_CLIENT link local: [undef]
Aug 28 19:58:51 homeLYnk daemon.notice openvpn[917]: TCP connection established with [AF_INET]40.118.18.71:443
Aug 28 19:58:50 homeLYnk daemon.notice openvpn[917]: Attempting to establish TCP connection with [AF_INET]40.118.18.71:443 [nonblock]
Aug 28 19:58:40 homeLYnk daemon.notice openvpn[917]: SIGUSR1[soft,auth-failure] received, process restarting
Aug 28 19:58:40 homeLYnk daemon.notice openvpn[917]: AUTH: Received control message: AUTH_FAILED
Aug 28 19:58:38 homeLYnk daemon.notice openvpn[917]: [serverSouth] Peer Connection Initiated with [AF_INET]40.118.18.71:443
Aug 28 19:58:34 homeLYnk daemon.notice openvpn[917]: TCPv4_CLIENT link remote: [AF_INET]40.118.18.71:443
Aug 28 19:58:34 homeLYnk daemon.notice openvpn[917]: TCPv4_CLIENT link local: [undef]
Aug 28 19:58:34 homeLYnk daemon.notice openvpn[917]: TCP connection established with [AF_INET]40.118.18.71:443
Aug 28 19:58:33 homeLYnk daemon.notice openvpn[917]: Attempting to establish TCP connection with [AF_INET]40.118.18.71:443 [nonblock]
Aug 28 19:58:23 homeLYnk daemon.notice openvpn[917]: SIGUSR1[soft,auth-failure] received, process restarting
Aug 28 19:58:23 homeLYnk daemon.notice openvpn[917]: AUTH: Received control message: AUTH_FAILED
Aug 28 19:58:20 homeLYnk daemon.notice openvpn[917]: [serverSouth] Peer Connection Initiated with [AF_INET]40.118.18.71:443
Aug 28 19:58:16 homeLYnk daemon.notice openvpn[917]: TCPv4_CLIENT link remote: [AF_INET]40.118.18.71:443
Aug
Best regards,
Koen
Accepted Solutions
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
Hello Koen,
Do not worry this is only activity from Camel project (Cloud connections) and no hacking activity.
Sincerely,
David