SpaceLogic KNX Forum
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Unfortunately I can't install it
Greetings Sebastian
Link copied. Please paste this link to share this article on your social media post.
Hi Sebastian,
seems on your screen is a message that signature is not correct. Can you tell me what firmware version are you upgrading to which one? Also you must be on production firmware as if you are for example a betatester the signature in your controller is different.
Link copied. Please paste this link to share this article on your social media post.
I’ve got the same error message. I’m upgrading from 2.8.3 to 3.0.0.
Link copied. Please paste this link to share this article on your social media post.
Hi,
Unfortunately I can't install version 3.0.0 either on wiser for KNX.
I'm prompted with the same message: Cannot upgrade, firmware image file is invalid.
i have installed the firmware version 2.8.3.
Link copied. Please paste this link to share this article on your social media post.
What type of controller do you have? homeLYnk, Wiser for KNX or spaceLYnk? What Hardware version? Do you see a reset button on the front below the LED’s ? What is the full name of the 3.0.0 FW you are attempting to install at the moment?
Link copied. Please paste this link to share this article on your social media post.
@Erwin-vd-Zwart My controller is the LSS100100 Wiser for KNX.
Name of Firmware next:
Wiser for KNX firmware V3.0.0 (Hardware 2.X.X and hardware 3.X.X) (V3.0.0)
Thanks
Link copied. Please paste this link to share this article on your social media post.
As requested above:
What Hardware version do you have (mentioned on the side of the controller)?
Do you see a reset button on the front below the LED’s? (Yes= HW 2 or 3, No = HW 1)
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.