Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

scene store script like in the old PICED C-Bus programming software

SpaceLogic C-Bus Forum

Schneider Electric forum about the C-Bus platform to get support and share knowledge including Network Automation Controller (NAC), Application Controller (AC) at selection, installation and troubleshooting sides.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic C-Bus Forum
  • scene store script like in the old PICED C-Bus programming software
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
sesa96364
sesa96364 Leader
9
KCWong
KCWong Troubleshooter
5
Mr_C
Mr_C Troubleshooter
3
View All

Recommended Forums

  • Intelligent Devices Forum

  • SmartConnector Forum

  • Metering & Power Quality

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to SpaceLogic C-Bus Forum
Start a Topic
Coppo
Coppo Mentor
Mentor

Posted: ‎2020-09-28 07:12 PM . Last Modified: ‎2026-05-12 06:00 PM

0 Likes
0
977
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
‎2020-09-28 07:12 PM

scene store script like in the old PICED C-Bus programming software

for replicating the "scenestore button" from old touchscreens / 5500PACA that used PICED C-Bus programming software.


===================================================================

configuring the "trigger object" 

configure the "visual object - triggering button" with  standard on/off properties,  the lua script will reset the trigger object's status and also act as an visual indication that the “lua code” operated...
...for example...  when the the lua code runs it will set the "triggering object/button" to "off" state.


--------------------------------------------

***Assuming that you have already created the required scenes in the "Scenes" Tab in your controller.  


1/ create a visualisation page for the specific scene you wish to store.

2/ add slider or dimmer object for each GA you wish to store in the scene.
   This will allow the enduser to do easier scene editing.

3/ add an extra visual object on the page that can be used as "scene store" button.

4/ create a event based lua script using the code below,
    some of the code will convert itself to comments when pasted into the NAC/SHAC script window.

"--" characters turn text into comments  FYI.

code is using local nertwork "0", application "56", Group address "1",  to 'run the lua code'.   
---------------------------------------------

--event based lua script for scenestore function
if GetCBusState(0, 56, 1) == true --create a "scene store" page and use a on/off button with this example GA=1 and label the button as "store Scene 1"
then
StoreScene("Scene 1") -- Enter the name of the scene you wish to store in " "....ie Scene 1
SetCBusState(0, 56, 1, false) -- Reset the button / GA used to triggger the Scene store function...ie GA=1
end

Tags (5)
  • Tags:
  • 5500AC2
  • 5500nac
  • 5500NAC2
  • 5500shac
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.