5 Reasons to Choose Circuit Breakers Over Fuses

Solutions for Motor Management

Get support to configure, troubleshoot, update or upgrade your motor management solution built with Altivar variable speed drives and Tesys devices to start, control, protect and monitor Low Voltage and Medium Voltage motors and loads, covering direct start, soft start and variable speed control.
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
  • Industrial Automation
  • Solutions for Motor Management
  • 5 Reasons to Choose Circuit Breakers Over Fuses
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BJacqz
Commander BJacqz Commander
49
LeoLazzaro
Lieutenant LeoLazzaro Lieutenant
16
PriscilaCunha22
Lieutenant JG PriscilaCunha22 Lieutenant JG
15
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Solutions for Motor Management
Start a Topic
ClaudiaCombei
Crewman ClaudiaCombei Crewman
Crewman

Posted: ‎2021-03-25 09:01 AM . Last Modified: ‎2021-03-25 09:11 AM

5 Likes
0
2171
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
Posted: ‎2021-03-25 09:01 AM . Last Modified: ‎2021-03-25 09:11 AM

5 Reasons to Choose Circuit Breakers Over Fuses

In the beginning, only fuses were used in electrical distribution systems to protect people and equipment against short circuits, circuit overloads, and other types of faults. Then, circuit breakers were introduced, offering many advantages over fuses.

For processing and manufacturing operations, protecting motors is crucial to maintain productivity. As the cost of a fuse is typically much lower than a circuit breaker, fuses have often been the choice for this application.

Comparing modern circuit breakers to fuses reveals how circuit breakers can help machine manufacturers and facility management teams achieve greater safety and reliability, lower costs, and support for energy management initiatives.

 

Consistent performance 🏆

post.jpg

 

One downside of fuses is that their performance can degrade due to aging, even causing them to open during normal conditions. In addition, there is no way to test a fuse, so you will never know the exact current value that will cause it to open. In contrast, circuit breakers are tested during manufacture and can also be retested during their ope

rating life to ensure performance is maintained.

 

Extended protection 🛡

The breaking capacity of a circuit breaker can be greater than equivalent fuses (up to 150 kA). And under overload conditions, a circuit breaker can trip up to 1000 times faster than a fuse. Some circuit breakers also provide ex

ceptional fault current limitation, a capability previously associated only with fuses. This not only supports reliable protection, it also reduces asset aging and extends service life. Another aspect of protection to keep in mind is that it’s common for only one of three fuses to open, causing a motor to continue running

 on two phases, as well as potentially experiencing an overload. This will never happen with a circuit breaker, which will always break all three phases simultaneously.

 

Enhanced safety and uptime 🎯

The use of fuses can represent a safety risk for technical personnel. Due to exposed conductors, replacement of fuses can be dangerous for unskilled people. The connections to circuit breakers are hidden behind the device, and operation can be done remotely. This makes breakers safer, especially for unskilled workers. One of the reported causes of fires in industrial environments is a fuse that has been replaced with the wrong model or rating, or even with wires or paper clips. These kinds of mistakes are avoided with circuit breakers, as they usually do not require replacement after a trip. Additionally, replacing fuses takes more time than simply reclosing a breaker. This means circuit breakers help minimize downtime and production losses.

 

Cost savings 💰

As mentioned above, the cost of a single fuse is significantly less than the cost of a circuit breaker. However, when we consider the complete cost of an installation, there are other costs that need to be taken into account. First, of course, is that three fuses are required for a three-phase circuit, with each fuse requiring the cost of a fuse base. Second, unlike circuit breakers, fuses do not have any built-in switching capability, so the addition of an upstream switch is required. Fuses also require a larger enclosure, due to their heat dissipation. And finally, when one of three fuses opens, all three fuses should be replaced. This requires an expensive replacement stock of fuses to be kept on hand. So, in total, the complete cost of using fuses can be greater than a circuit breaker. Though occasional replacement of circuit breakers may be necessary, a single model of breaker can usually be used for different power ratings, which minimizes inventory.

 

Greater functionality ✔️

Unlike fuses, circuit breakers can be enhanced with additional functions, such as ground fault protection. They also allow for system coordination between breakers (e.g. selectivity, cascading). The newest, most advanced circuit breakers offer a large breadth of capabilities in a compact size with flexible designs that enable field-upgrading. Add-ons can include remote control and status indication, alarm and auxiliary contacts, power and energy measurements, and network communications.

 

 

Click here to learn more about solutions that can help protect your entire machine application, not just the motor.

 

Labels
  • Labels:
  • Best Practice
  • Design & Build
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.