Issue installing SmartConnector with LocalDb on same machine as EBO Enterprise and License server
Has anyone had an issue installing SmartConnector on the same machine as the EBO Enterprise server and License server? For me, it doesn't seem to install (or uninstall) correctly and I believe it to be a conflict with the use of SQL local db.
The local data base files get created on installation, but the log indicates that the username and password used for installation is in correct, even though they are correct.
When the services starts, I cannot connect to the portal, i see this error in the log "PortalAddress disabled because there is no defined endpoint", indicating that the db hasn't been configured correctly.
When i try to uninstall, i get an error saying that the local db files are in use.
Is this a known issue or could it be something else??
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
is the db being created in sql?
can u connect to sql in management studio or odbc?
search for the smartconnector success kit on this forum. it may help you solve this.
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
Hi Daniel, this only seems to be an issue when using localDb and EBO has already been installed. When using SQL, it is not an issue.