GET /Containers not work
SmartConnector + EBO3.0
When I use GET /Containers in swagger ui, it did not work.(It works with SBO1.9)
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
Hi Xiangfeng,
It looks like you have configured an SboEwsRestProvider (based on the error you are showing). This provider tends to be pretty quirky, and with EBO 3.0+ there are some incompatabilities and it is not recommended to use unless there is a very specific need.
Please try and reconfigure a new endpoint using the SoapEwsRestProvider and try this again, however just as a note, with the SoapEwsRestProvider the supported way to search for objects is with the /Containers/{id}/Children endpoint.
Best Regards,
-Jeff
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
Hi, Jeff
I have reconfigured another endpoint. But the problem still exists.
And GET /Containers/{id}/Children method, the filter is not work.
For example, when I set type=Trend, all the items include Values, Alarms,Containers,etc. still return.
BR,
Su
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
Hi Xiangfeng,
I tested this locally, and I cannot reproduce what you are seeing.
Please send me an email at jeff.bowman@se.com
Best Regards,
-Jeff
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
SmartConnector 2.4.23 + EBO v3.0
1、With SboEwsRestProvider: GET /Containers not work, GET /Containers/{id}/Children the filter not, that is not matter what the filter is(Trend, Value), It will response all items.
2、With SoapEwsRestProvider: GET /Containers/{id}/Children, the filter works well.
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
1、the problem: GET /Containers does not work in EBO 3.0(Work in SBO1.9) have the same problem with the method Retrieve(query) in CspClient.
The method Retrieve just support SBO, not EBO.
2、problem: GET /Containers/{id}/Children does not work in SboEwsRestProvider has the same problem with method GetChildObjects in CspClient.
the cspTypeFilter does not work well.