Differentiate log files
Hi everyone,
I have created several smartconnector processors running in the same Server.
Is it possible to create different log files?
For example "SC1_YYYY-MM-DD.log", "SC2_YYYY-MM-DD.log", etc.
Thanks
BR
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
With C# you can create whatever you like (:
But when using the default log classes i don’t think you have that option, you can however add your processor name into the log entries so you can filter them out more easily..
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
Thanks Erwin.
I have already entered the names, but there are so many logs.
I wanted to know if it was possible with the default class. Otherwise I use another one.