Posted: 2024-12-28 12:13 PM
wiser hub only - is it possible
i am looking for a simple solution to turn the combi boiler on when out of the house - the 1/2/3 hour boost would answer that question but is that possible without a thermostat in the system - can i set the system up via the app without a thermostat as it is something i wont use - i also dont need to program the heating - i prefer manual control
if thats not possible could i add a trv head and then get access to the app - i have a number of drayton trv's so assume a head would fit one of those - would prefer not to have either a stat or trv head though
thanks
- Labels:
-
Apps
-
Temperature Control
- Tags:
- english
Authentication Failed.
- Authentication Ticket Mismatched, failed authentication.
Link copied. Please paste this link to share this article on your social media post.