Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2018-03-0708:29 AM. Last Modified: 2022-02-1104:59 AM
Wiser Smart Thermostat application note
For proper functionality and long battery life it is necessary to keep these installation rules
1) Wiser Smart Controller shall not placed beside wi-fi router
2) Thermostat shall be on place where customer can see status of device
3) All devices in the system must be properly commissioned - H-relay cannot be alone in a zone. Always with Thermostat
4) Controller must be ON all time. If necessary to switch off then batteries from Thermostat need to be removed
5) Mains-powered Wiser Smart devices must retain ON all the time as they work also as Zigbee signal extenders (H-ACT, L-ACT, SmartPlug). If there is active any 3rd party system switching off power branches, this must be deactivated.
7) Keep in mind distance between battery and socked-powered devices. Walls, ceilings or floors significantly reduce zigbee signal strength.