Ask our Experts
Didn't find what you are looking for? Ask our experts!
Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-09-28 12:24 AM . Last Modified: 2025-09-28 04:50 AM
We have a Worcester Bosch 18 RI boiler (non-open therm) connected to a Wiser Gen 2 thermostat. We noticed that the thermostat would ask the boiler to come on and go off every 10 minutes. We spoke with the UK support team, who explained that this is an industry standard for all smart thermostats. They advised that we use the Heat Pump mode to overcome this.
We have now set the system to heat pump, and yes, it works like a normal thermostat - however, we have lost all of the INSIGHTS information....... and the support team do not seem to want to know.
Most houses in the UK (except for the ones built in the last 10 years) will have their GSH sized on the maximum output of the radiators which mean that they must be upto normal operating temperature e.g. 60 or 70 deg. cel. When you cycle a boiler every 10 minutes the radiator does not have time to warm up as it take 3 minutes for the boiler to run through is warm up procedure before fully opening the gas valve. leaving only 7 minutes to heat the house up.
Running a boiler in this was is not only very inefficient (the water pump is working for an excessive time (our electric consumption dramatically increased) but is also creates excessive wear on the boiler (feedback from British Gas). It also means the house does not come up to temperature...............
This system is not cheap and we choose it because of the INSIGHTS data which we are now are no longer able to see. Any help or assistance would be greatly appreciated.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-09-30 02:19 AM
Hi @OKC171166 ,
Thanks for your message. For Insights issue, did you make the operations described here ?
If you continue not to have Insights displayed, please contact the local customer support for assistance.
Concerning the "heating" questions, when cycling is set to 10 mins, it doesn't mean necessarily that the boiler will stop every 10 min.
If the heat demand is important, meaning that the current temperature is mush lower than the set point, the Wiser system will instruct the boiler to fire all the time, until the set point is almost reached.
Once the temperature is close to the set point, Wiser will reduce slightly the boiler's cycle to avoid overshooting the set point.
Finally, Wiser will stabilize at a cycle where the current temperature is almost equal to the set point.
Best regards.
David
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-09-30 11:43 AM
David, thank you for your reply. When set to a Gas boiler, it always seems to fire every 10 minutes and off for 10 minutes, even when the set temperature is more than 2 deg. cel. more than the actual. Are you saying that this is correct? The boiler takes 3 minutes to run through its start-up sequence before it fully opens up to full capacity, e.g., the burner. increases. This does not allow the radiators to even get warm and even now the house does get warmer (it is very mild weather in the SE of the UK). The UK support team have told me to use the "Heat Pump" setting and this keeps the boiler firing until the set temperature is reached BUT it stops the INSIGHTS page from working. Does Insights work with the HEAT PUMP setting?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-06 05:58 AM
hi @OKC171166 ,
Thanks to come back to us, please can you share here the Zendesk ticket provided by the UK support team ? Then we can have a look on your system behaviour.
Thanks.
BR
David
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-06 10:59 PM
That’s interesting! The UK support team told me to do the same, and my Insights is still working perfectly. Are you using Insights or Insights+?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-25 10:58 AM
No, my Insights (Heat Report is blank). Even when there is a 2 or 3 degree difference in the set temperature and the actual, it still fires every 10 minutes, then off for 10 minutes. The UK support team are not assisting at all - very frustrating.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-26 09:36 AM
I seem to be having same issue. I have an Ideal boiler that appears to be short cycling.
I saw on another post a suggestion to change the setting to 'Oil Boiler' please explain difference in the Gas, Boiler, Oil Boiler and heat pump settings,
Surely there should be a proper solution to this rather than a fudge!
Thanks
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-28 08:30 AM
David, can we deal directly with yourselves, as the UK support clearly does not understand or care, as they have not offered any solutions apart from the fact that we have to use the heat pump setting - they ignore the fact that Insights is missing (which is why we purchased the system). We have spent hours on the phone with them and do not get anywhere. Can we have a standard boiler setting with Insights?Dave.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-28 08:33 AM
David, Can you provide details on the temperature differences and the firing/non firing periods so that we can test our system.?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-30 02:47 PM
Hi @OKC171166 ,
I don't know if you already have it but you can refer to the Wiser Home system user guide here ?
Based on your configuration you can have access to further information on settings.
If you don't find it, please come back here and i will try to support but the better way is with your local customer support as they are able to consult your configuration.
BR
David
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-11-01 08:07 AM
David,
I have tried to go through the local support team, but they seem to be unable to answer the simple question regarding the settings. They have logged into my system in the past and looked at the settings and all they do in advise to set it to Heat pump - they do not seem to know anything about the integration settings (e.g. 10 mins on 10 mins off). It does appear that even with a very large temperature difference of 7 deg Cel. the standard boiler setting is 10 mins on 10 mins off. Nobody seems to give a simple answer to this problem which is when you are forced to set it to anything other than Gas boiler you loose the Insights data.
The 10 min on and 10 mins off is totally inappropriate for most boilers as it does not take into account the start up time etc and allow sufficient time for the boiler/radiator to reach optimum temperature - most houses do not use low temperature radiators but high temperature rads.
Can you please explain the integration settings of the "Gas Boiler" setting WRT the integration and also how the heat pump and oil boiler settings also function as there is NOTHING in the manual to explain any of this.
We have spent a lot upgrading to this system after being sold on the different functionality but it appears that we are not able to use it due to having to have our system set to a Heat pump because it will not work when set to a gas boiler.
Is it not possible to have a ther device setting for a gas boiler that is purely for old conventional boilers that can also capture the Insights data. Please can you put this forward to the development team?
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.