Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-12-31 05:36 AM
Hi all,
I've been using the Wiser smart heating system in my home for about a month now. It's a three-storey house with the Heat Hub R located next to a combi boiler in the middle of the top floor. We have a BT mesh WiFi system with very fast WiFi signal. All BT discs in the house are connected to the main router by ethernet cable, so the WiFi system is very stable. The Wiser room thermostat is wall-mounted in the hallway on the middle floor. I've installed Wiser smart radiator thermostat valves on three radiators on each of the top floor, middle floor and ground floor, i.e. nine valves in total. I have an iPhone and my Wiser Home app is operated via that. I don't use Google home assistant or Alexa and I'd prefer not to add those layers of complication if I can avoid it. Likewise, I don't operate any other home appliances, lighting, etc in a 'smart' way - I just wanted more control over my heating in a fairly large house that's often minimally occupied.
My initial impressions of the Wiser system are positive. I experienced some losses of connection between the app and the main Hub R to begin with but that's largely settled down now. The other niggly issue has been individual radiators losing connection to the main hub, i.e. a 'no signal' error meaning you lose the ability to control them except manually at the valve. Generally these valves re-establish connection after a while but sometimes it's taken half a day or more; or I've had to power them down and force a reconnect.
Having noticed that the radiators most prone to losing connection with the hub are the ones in the rooms at the front of the house, I decided to buy a Wiser Smart Plug to use as a range extender. The front/middle floor room is reasonably close to the main Hub R, so by using an electrical socket in that room I figured the smart plug should act as a bridge for the three radiators in the front rooms on the top, middle and ground floors that have had less stable connections.
My Wiser smart plug has product number WB704H1A0902 and the paper instructions/quick start guide inside its box have a matching number.
I've searched this forum and saw this thread:
...which is along similar lines to my own queries, but only partially answered them and/or did so in a way that was a bit too techy for me. So I hope someone may be able to provide some help with the issues I'm not sure about. Here goes:
1. I set up the smart plug as per the instruction guide, including powering down the Hub R for a couple of minutes. I hope it's worked as planned but Just to repeat comments made by others on here: it's frustrating not to be able to tell how my new plug is being utilised (if at all!) by my Wiser system. All I know is that the plug has appeared as a connected device on my app home page. Am I right in thinking that (without employing techy software as suggested in the thread posted above) I just have to hope for the best that my 'weak signal' radiator valves will latch onto the newly installed plug?
2. The plug setup guide tells me I can check the RF signal strength of the plug in the Wiser Heat app by going into 'Settings' and then the 'Devices' category. That just seems to be flat wrong, unless I'm missing something. I'm confused as to why the Wiser guide says you can do it, and gives specific instructions how, but it seems there's actually no such facility in the app?
3. I can turn the smart plug on and off either manually using its button or remotely via the app. In either case, when it's turned on a solid blue light appears on top. If the plug is turned off (no light visible) does that mean it's totally inactive as a range extender? If that's the case, then basically I'll need to have the smart plug switched on more or less 24/7 unless I schedule it to come on and off at the same times as the 'target' radiators?
4. ...and if the hypothesis at 3 above is correct, i.e. the plug only works as an extender with the blue light switched on, then I have an extra issue since I'm hoping the plug will stabilise the hub connection for three separate radiators which are all programmed to have different on/off schedules. So I could elect to apply to the smart plug the same schedule as the radiator on the front/ground floor, which is scheduled to be on more often than the other two, but that would still leave some mismatches when other 'weak' rads are in use but are not getting the benefit of the plug extender. Or, I guess I could just programme the plug to be 'on' from early morning until after normal bedtime so that it's always available for any rad that needs it? Not a major drama if that's the case, but I'd like to understand if that's how it has to work
It's too soon for me to judge whether the plug is having the desired effect on keeping the 'weak' radiator valves connected to the hub. I'll happily report back on progress. But initially I'd just like to get reassurance that I've understood how the system works with the range extender plug, or (if I haven't) get some clarity on what I'm missing!
Sorry the above is so wordy but - as a non-expert home tech user - I've found that reading other people's descriptions of their own home setups, and their own issues and queries, plus the thoughtful responses of those who are more techy or experienced, enormously helpful. So here's thanks in advance for anyone kind enough to respond.
Cheers.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-01-05 03:02 AM
Yup you've nailed it. the socket needs power to act as a extender and aftewr that it 's just a plug socket with a blue light to tell you if it's on or off. No need for schedules unless you specifically wnat to turn something on or off at a certain time
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-01-03 02:19 AM
I think you'll find the instructions included with the smart plugs are unfortunately a bit out of date. I have three of the plugs and I just paired them in the app the same as you would as TRV. I did power off the the hub.
The blue light just tells you that the socket is on smae as if you had illuminated wall sockets. As long as you have power going into the smart plug it should be connected to the hub and TRV's will connect (and disconnect) to it as they see fit.
I run home assistant with the wiser integration and there is a "card" in there which shows me the connection of the entire wiser network. so I can at least confirm it works
despite what the instructions may say there is no signal strength indication between the plugs and the hub like there is with the the TRV's.
It's not the best implementation by wiser there is work still to do but it does work.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-01-04 03:45 AM
Hi Brian
Thanks very much, that's really useful and it's interesting to see how your home assistant illustrates your home setup and what's connected to what (I assume that's where your screenshot came from). It would be great to have that facility within the Wiser app but, as you say, maybe that's something for the future.
So - just for clarity, and for the next 'me' that reads this - I think what you're saying is that, if you're only using the smart plug as a range extender for the Wiser heat system, once the smart plug has initially been linked to the hub there's no need to ever have the smart plug switched 'on' with the blue light shining? In other words, it will perform its function of boosting the Wiser heat network just by being paired to the hub and then passively left plugged in.
Presumably, if you were using the smart plug to control an appliance like a lamp (which I'm not) then you would need to switch on the smart plug, or schedule it to switch on, at the time you wanted the lamp to turn on and the plug's blue light would then come on at the same time as the lamp. Correct?
If all the above is correct, then it follows that I don't need to assign any timing schedule to my smart plug in the Wiser app? Until I read your post I'd set up and was using a schedule for the smart plug so that it turned on at the same time as its 'target' radiators in the morning and then off at the end of the day when all heating was turning off. But it seems I can just have the plug 'off' 24/7 but (while it stays connected to the hub) it'll do its extender job regardless.
Since I first installed the smart plug at the weekend I haven't spotted a single drop-out of TRV connection on the three radiators that previously had been prone to losing connection with the hub, so it does seem to be working well. After reading your post, I've switched off the plug (no blue light) and have disapplied my on/off schedule for it on the app. Hopefully that won't alter the stability of the extension setup - the proof should come over the next few days as I monitor potential connection losses on the affected radiators.
Thanks again. If you can spare the time to say whether I've correctly summarised your advice above (or in what way I haven't!) that would be fab.
Cheers. LWU.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-01-05 03:02 AM
Yup you've nailed it. the socket needs power to act as a extender and aftewr that it 's just a plug socket with a blue light to tell you if it's on or off. No need for schedules unless you specifically wnat to turn something on or off at a certain time
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-01-06 03:51 AM
Thanks again. Super-helpful.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-30 08:38 AM
Hi, I'm new to Wiser, less than a week with 1 x HubR 1 1 x Room Stat and 10 TRVs. All seem to now be working as I want them, but the 3 TRVs in the bedrooms have a weak signal and drop out every now and then. I have brought an extender, and it is installed upstairs, but the TRVs in the bedrooms do not appear to have any stronger signal now and want to know whether your home assistant will show whether the TRVs are connected to the extender. So my questions are 1) which "Home Assistant" are you using and 2) does it show if the devices are connected to the extender? Thanks and hope you and let me know
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-10-02 02:15 AM . Last Modified: 2024-10-02 02:16 AM
Yes the home assistant can show what is connected to either the hub or the extenders using the ZIgbee card. they connections do like to hop around a bit though. I have a trv in the same room as an extender but it's not connected to it. but a trv in another room is. You may find that although your exteders are up and running the TRV's as yet haven't connected to them, tomorrow however they may have done. you could try killing the power to the hub for a minute and then letting them all find their strongest signal, that could work.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-10-02 10:40 AM
Many thanks, I will keep monitoring, and with winter coming I may investigate setting up my own Home Assistant machine
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-03-13 05:56 AM
I see this topic (which I started in 2023) has had quite a few views, so it might be helpful if I add an update.
I really like the Wiser Home system but from time to time I would have spells of "unable to connect to your hub" failures when using the app on my phone, and it was also fairly frequent to get notifications that individual raditors were offline (i.e. not connected to the hub), albeit these issues usually fixed themselves after a while.
At one point early this year, though, the connectivity of the phone app with the hub was getting really sketchy and I had to contact the Help Centre and ask them to take a look at it. As a result, basically I reset the app from scratch (with their help) and things did improve somewhat after that, but the same kind of issues were still happening quite often.
One thing that had been nagging at me was that the "strength of connection" symbol for the main Heat Hub R to my WiFi system (which you can find in Devices within Settings on the phone app) was often only at two bars. I'd always found that a bit surprising because the house is set up with a BT Whole Home mesh and for usual purposes the WiFi signal is pretty good anywhere in the house. Having said that, our Wiser hub is located in a bathroom on the top floor, inside a cupboard that houses the central heating boiler.
So, I bit the bullet and ordered an additional BT WiFi extender disc, which I located as close as I could to the Wiser hub (just the other side of a stud partition wall from where the hub is fixed). The WiFi connection indicator for the hub instantly showed a full four bars and has remained at that level ever since. That was about a month ago now and since that time there hasn't been a single instance of my hub dropping off the system, i.e. no "can't connect to your hub" error messages in that whole time.
Just as interestingly, the connection strength indicators for each individual radiator, as shown on the app, have been greatly improved from previous levels since I added the BT disc to the house WiFi system. They're all now showing as strong or good, whereas some used to show as weak connections. In the month since the disc was added, there's only been one single instance of a radiator briefly going offline, whereas it was happening pretty regularly before that. I'm confused as to what's going on here as I'd understood that the radiators connect through a zigbee network, rather than using the house WiFi. In which case, I'm not sure why the radiators should now be more stable than they used to be? Perhaps someone more tech-aware than me can explain this improvement, assuming it's not pure coincidence (which seems unlikely as it happened simultaneously with the WiFi improvement and has sustained for a month now).
In any event, and I hope I'm not jinxing things by posting this, my whole system now seems way more stable (flawless, in fact) since I took steps to ensure that the main Heat Hub R had a rock-solid WiFi connection. So anyone else finding the app's connectivity a bit flaky might want to consider whether they have the ability to solidify the link between their hub and their home WiFi network.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-25 05:20 AM
Looking at https://www.se.com/uk/en/faqs/FAQ000208303/ it looks like zigbee uses the same frequency as 2.4Ghz Wifi. So maybe the additional WiFi extender made the WiFi mesh change the frequencies it was using and which meant that the zigbee network has less interference? I am just guessing! I was just reading through this posting to try and work out if I should get a Wiser Extender as two of our radiators regularly go offline.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-10-30 03:01 PM
Hi @dwbuk ,
First, you can use the device Zigbee strength info in the Wiser Home app to obtain an idea of the RSSI (Received Signal Strength Indicator) then you can decide if you need to add an extender or not.
Please note that you can add a smartplug betwween radiators and hub to improve the signal strength.
BR
David
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.