RemoteConnect Replace Variables Does Not Work SCADAPack X70
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2023-04-0412:32 PM. Last Modified: 2023-04-0412:33 PM
RemoteConnect Replace Variables Does Not Work SCADAPack X70
I've got a problem with RemoteConnect where I need to change the logic variable and modbus data type for many objects. I export the project to an excel file, make the changes, then import the modified excel file. When I try to build the logic and download to the PLC I get an error that the logic editor is missing variables for objects in the object data base. The error message says to use the Replace Variables button to replace them. I can press this button but it doesn't seem to do anything and the error persists. I've tried the import/replace with the logic editor open and closed. With the editor open I don't get the usual prompt to accept the changes and when the editor is closed no changes seem to be made.
I can change the data types from remote connect and that seems to work most of the time but there are a few problems. First, there are a couple hundred objects that have to be changed. Second even when I am changing them from RemoteConnect every once in a while I get the same problem where the change doesn't get pushed to the logic editor and the Replace Variables button doesn't fix it.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-04-1307:39 AM
Probably best to have a chat with our Tech Support team about this issue. You can find contact information by going to se.com and opening the Support menu. Select Contact Support then the information will be available once you've selected your region.
Joel Weder Remote Operations Specialist Schneider Electric