Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Realflo Flow Computer 7.10.2: Now Available for download from Exchange Shop
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2022-07-0605:07 AM. Last Modified: 2022-11-2808:00 AM
Realflo Flow Computer 7.10.2: Now Available for download from Exchange Shop
Hello Remote Operations Community,
We're pleased to announce the release of Realflo Flow Computer 7.10.2 for SCADAPack Smart RTUs, comprised of the following new features, improvements and fixed issues:
New Features:
Logging of M (Meter) Factor and K Factor can be suppressed for AGA-7 and AGA-9 configuration commands. This reduces the number of logged changes when frequent updates are made to the factors
.
Improvements:
Three permission controls were added to the Device Lock permissions. These permissions are available when locked: Calibration/Forcing, Realflo Accounts, and Run Execution Control.
Fixed Issues:
Realflo could not log into the ADMIN account after using another account. This is corrected.
Realflo did not update the stored PIN if the PIN was changed outside the Realflo application and accounts were later read back by Realflo. This is corrected.
Status code 30027 (User is not authorized to perform this function) was returned when changing the ADMIN account pass code from an ADMIN level account. This is corrected.
Application and Flow Computer Versions Contained in this Release:
Realflo application version is 7.10.3367
Flow computer version is 7.10.3367 for SCADAPack 32, 300 series, x70, and 4203 Flow computer version is 7.01.90 for SCADAPack 16-bit controllers
The software package is available for download from Exchange Shop: