Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

[Imported] Telnet & Hyperterminal not available in Win7 & newer

Remote Operations Forum

Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.​
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
  • Remote Operations
  • Remote Operations Forum
  • [Imported] Telnet & Hyperterminal not available in Win7 & newer
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Joel_Weder
Captain Joel_Weder Captain
92
BevanWeiss
Spock BevanWeiss
24
sbeadle
Kirk sbeadle Kirk
17
View All

Recommended Forums

  • EcoStruxure Geo SCADA Expert Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Related Products
product field
Schneider Electric
Trio Licensed Radios

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Remote Operations Forum
Start a Topic
sbeadle
Kirk sbeadle Kirk
Kirk

Posted: ‎2019-10-25 12:27 PM

0 Likes
0
826
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
Posted: ‎2019-10-25 12:27 PM

[Imported] Telnet & Hyperterminal not available in Win7 & newer

>>Message imported from previous forum - Category:Trio Data Radios<<
User: joelw, originally posted: 2018-10-16 21:43:16 Id:36
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

---------------

**_jweder:
The Trio J Series Ethernet radio can be configured & diagnostics run either using the web interface or a text based interface. Many users prefer the text interface as it is quicker and less bandwidth intensive than the web interface._**

_________________

With Telnet, either via the command line Telnet tool or via Hyperterminal, the user can access the text interface via a radio's LAN port or over the air. This is the quickest way to talk to a radio. As long as you know its IP address you can work very efficiently. And even if you don't know the radio's IP address you can still talk to the radio's text interface (by default) on serial Port A, at 19200 8N1.

Yet in Windows Vista and Windows 7 computers the required Hyperterminal or command line Telnet software is not by default available. What can you do?

In fact you have several options. One is to enable Telnet (yes it IS in Win7 and Vista, just hidden!) Here's how:

1. Click on Start
2. Click on Control Panel
3. Go to Programs or Programs and Features as required
4. Click Turn Windows Features On Or Off
5. In the Windows Features dialog box, tick the Telnet Client check box
6. Click OK

Many people are not aware that Hyperterminal has the inherent ability to perform Telnet communications. Yet this functionality has been available for years. All you need, to do either serial or Telnet communication, is a copy of Hyperterminal or a similar program.

You can purchase Hyperterminal "Private Edition" from the Hilgrave website: http://www.hilgraeve.com/hyperterminal.html for (currently) about $60 USD. Not a bad deal, but if you still have a Windows XP machine you can simply copy your existing Hyperterminal files to the new computer.

Required files are:
- hypertrm.dll Found in C:\\Windows\\System32
- hypertrm.exe Found in C:\\Program Files\\Windows NT

Simply copy those files into any directory on your machine and it will work.

If you'd rather use another terminal program, try PuTTY. Here's some very basic instructions:

1. Go to http://www.chiark.greenend.org.uk/~sgtatham/putty/download.html
2. Download Windows Installer file putty-0.60-installer.exe (or newer)
3. Install the file, allowing it to install in the default location.
4. Run PuTTY. The default Connection type is SSH.
5. Change the default to Telnet. Type the radio's IP address. Port 23 is ok.
6. Click Open to begin a session.
7. OR change the default Connection type to Serial, enter the desired serial port and baud rate, then click Open.

Labels
  • Labels:
  • Radio
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.