[Imported] Accutech custom data display?

Remote Operations Forum

Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.​
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
  • Remote Operations
  • Remote Operations Forum
  • [Imported] Accutech custom data display?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Joel_Weder
Captain Joel_Weder Captain
92
BevanWeiss
Spock BevanWeiss
24
sbeadle
Kirk sbeadle Kirk
17
MartinChartrand
Captain MartinChartrand Captain
15
View All
Related Products
product field
Schneider Electric
Accutech

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Remote Operations Forum
Start a Topic
sbeadle
Kirk sbeadle Kirk
Kirk

Posted: ‎2019-10-25 02:52 PM

0 Likes
0
1365
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
Posted: ‎2019-10-25 02:52 PM

[Imported] Accutech custom data display?

>>Message imported from previous forum - Category:Accutech<<
User: mchartrand, originally posted: 2018-10-17 19:25:38 Id:95
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

-------------------------------

**_PF533:
I work for a trade school. We have some Accutech devices that have been installed in an operating equipment lab and a BR-10 radio. They asked me to make it all work.
Do we have to add a Scadapack to be able to use the clearscuda host software to create our own display? Or can we just connect the radio to a PC running the scadaserver and the clearscada host software?????
We would like to be able to take the data and display it along with a representation of our processes on a large LCD Monitor in the lab and on PC's in the classroom. Where do I start??????_**

_________

WayneJohnston:
You don't need a SCADAPack to communicate with the BR10. You can connect ClearSCADA to the RS-485 Modbus port - with the right hardware on the PC - and poll readings from the base radio directly.
You can use Accutech Manager to configure the field units. Or, you can do the configuration directly from the local display on the base radio and field units.
All the information you need is in the user manual. Look at the section Wireless Base Radios Modbus Communications.

_________________________

**_PF533:
I have been using ClearSCADA today and creating a display. I will be using Accutech Manager to set up the devices. Can I use a smart cable and connect it between the modbus output on the Br10 and our servers rs232 input or will I need a different piece of hardware?
On using ClearSCADA to poll the BR10 will it recognize that it is polling Accutech Data like the Brochure says or will I have
give it more direction?_**

____________

WayneJohnston:
You can use the SmartCable with Accutech Manager to set up the devices.
I have not used the SmartCable with ClearSCADA, so I cannot say for sure if it will function. I've used other RS-232 to RS-485 converters which work fine.
You will have to configure points in ClearSCADA to poll the BR10. It will not automatically recognise the base radio.

Labels
  • Labels:
  • IAN (Instrument Area Network)
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.