Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84245members
353345posts

Ethernet/IP Protocol

Remote Operations Forum

Collaborate and share knowledge on the extensive range of remote systems and devices, including SCADA radios and RTUs, on the Schneider Electric Exchange Remote Operations (formerly SCADA & Telemetry) forum. From commissioning SCADA integration devices and software, to enhancing existing installations or troubleshooting, connect with a global community of experts and users. Subscribe today.

Inderjit
Cadet

Ethernet/IP Protocol

Hello,

I was wondering if there is any way of running Ethernet/Ip Protocol on Scadapack 575?

Tags (1)
2 Replies 2
BevanWeiss
Spock
Spock
0 Likes
1
381

Re: Ethernet/IP Protocol

Currently not really.

Your best bet if you have a CMPLX/CLX processor is to use ModbusTCP on the PLC to expose this to the SCADAPack x70.  Then you can use the ModbusScanner on the x70 to read the data.

 

There was a topic in the requested improvements for the x70 to include an Ethernet/IP CIP driver, but as far as I'm aware no progress has been made on this from Schneider.

 

There was a possible option when the x70 were going to be able to have custom C/C++ code deployed on them, it would have allowed for the creation of a custom Ethernet/IP CIP 'driver' (it's not a super complicated protocol).  But the current situation is that this won't be available at all for the x70 series, and would only be available in x70i series (which aren't available in the market yet).


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
gibsongilbert
Crewman
Crewman
0 Likes
0
327

Re: Ethernet/IP Protocol

Thank you for the information and for the nice suggestion...

Gilbert GBWhatsApp