Use this portal to submit your innovative ideas to make Geo SCADA Expert and Devices such as SCADAPack, Trio and Realflo of greater value to you and to the SCADA & Telemetry community. Every idea will be individually reviewed by our team for merit and will be marked Under Consideration.
Search in
We know Accutech product line, is a family of instruments reporting to a Base Radio and user ( PLC or SCADA ) can read each instrument information using 10 double word registers. We can read temperature , pressure and also voltage or current to join into the accutech network any standard 4-20mA or 0-10V devices. BUT imagine if we can integrate into the Accutech Network a Modbus slave ( or modbus TCP/P ) device. Just only read or write 10 registers. We can incorporate in a wireless network many devices like Variable speed drives, other brands instrumentation , PLCs , Energy measurement..... The hardware to implement this idea exist already , is the BR20 or BR21, the only job to do is modify the firmware to use the serial ports to read 10 registers from the modbus device and transmit that to the Accutech Base Radio as other Accutech instrument. We will can convert to wireless any modbus device in the field or plant. This idea has a grate potential in the market, also against competitors, they are unable to do that. What do you think?
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.