Accutech Modbus Master gateway to read Modbus devices and incorporate into WiStar net


We know Accutech product line, is a family of instruments reporting to a Base Radio and user ( PLC or SCADA ) can read each instrument information using 10 double word registers. We can read temperature , pressure and also voltage or current to join into the accutech network any standard 4-20mA or 0-10V devices. BUT imagine if we can integrate into the Accutech Network a Modbus slave ( or modbus TCP/P ) device. Just only read or write 10 registers. We can incorporate in a wireless network many devices like Variable speed drives, other brands instrumentation , PLCs , Energy measurement..... The hardware to implement this idea exist already , is the BR20 or BR21, the only job to do is modify the firmware to use the serial ports to read 10 registers from the modbus device and transmit that to the Accutech Base Radio as other Accutech instrument. We will can convert to wireless any modbus device in the field or plant. This idea has a grate potential in the market, also against competitors, they are unable to do that. What do you think?
- Find more ideas tagged with:
- Accutech Modbus Master
- english
- scada
- SCADA app
- SCADA software
- SCADA tutorial
- Telemetry and SCADA
Link copied. Please paste this link to share this article on your social media post.